How to do auto reporting on end device?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to do auto reporting on end device?

1,896件の閲覧回数
randolfhu
Contributor III

Hi Sir,

Since Thread v1.0.0 doesn't support "observe" in COAP. So if we want to get temperature from end device. We have to send Coap request every time. I would like to know if there have any THCI command which can report it's temperature to gateway automatically?

Thanks

Randolf

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,692件の閲覧回数
jc_pacheco
NXP Employee
NXP Employee

Hello Randolf, right now this is not supported but could be implemented at application layer, sending a custom COAP message, you'd need to implement an interval timer that triggers a temperature message within the COAP callback.

0 件の賞賛
返信