How to do auto reporting on end device?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to do auto reporting on end device?

1,901 Views
randolfhu
Contributor III

Hi Sir,

Since Thread v1.0.0 doesn't support "observe" in COAP. So if we want to get temperature from end device. We have to send Coap request every time. I would like to know if there have any THCI command which can report it's temperature to gateway automatically?

Thanks

Randolf

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

1,697 Views
jc_pacheco
NXP Employee
NXP Employee

Hello Randolf, right now this is not supported but could be implemented at application layer, sending a custom COAP message, you'd need to implement an interval timer that triggers a temperature message within the COAP callback.

0 Kudos
Reply