How to bind using the JN-AN-1229 instance.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to bind using the JN-AN-1229 instance.

1,830件の閲覧回数
377086561
Contributor II

I want to implement two scenarios,

1   the first of all devices (including routing devices and terminal devices) to connect to our source device (coordinator)

     You can use code to tell me how to communicate between the source device and the target device? Just looking at the documentation using the interface is a bit difficult for me? Thank you


2    I want the coordinator to be a source device that can bind multiple groups. For example, a group of many lamps, a set of many temperature sensors, can you do this?mario_castaneda‌dheerajsawant@

タグ(2)
0 件の賞賛
返信
1 返信

1,716件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi,

Could you please look at the JN-AN-1220? 

The example implements binding and finding process, also you could see the reporting value.

Regards,

Mario

0 件の賞賛
返信