How to Enable Flash Protection on KW45?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to Enable Flash Protection on KW45?

2,442件の閲覧回数
jictannu
Contributor III

Hello everyone,

I am currently working with the KW45 microcontroller and need to set up Flash protection. I have reviewed the user manual, which mentions the existence of Flash protection mechanisms, but it does not provide specific instructions on how to configure them.

Could someone please guide me on the steps required to enable Flash protection on the KW45? Any code snippets or detailed explanations would be highly appreciated.

Thank you in advance for your help!

タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,415件の閲覧回数
nxf77486
NXP TechSupport
NXP TechSupport

Hello,

 

Thank you for contacting NXP support.

Sure the KW45 offer flash protection by protecting the application code and data in flash and also encrypt them. With the NVM Prince  XEX (NPX) this is a module inside the flash memory controller that allow to protect content of flash.

Please find the application note in this link that has an explanation on how this work and how to enable this.

0 件の賞賛
返信

2,248件の閲覧回数
LiuYi
Contributor I
Hello,
The link you mentioned above is not accessible. Could you please provide it again?
0 件の賞賛
返信