How does the terminal node send data to the coordinator node?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How does the terminal node send data to the coordinator node?

2,896 Views
jun951753jun951
Contributor III

I successfully sent the data to the coordinator on the routing node, but failed to send the data on the terminal node using the same method.This is my sending function...

1.png

2.png
3.png
0 Kudos
Reply
3 Replies

2,762 Views
jun951753jun951
Contributor III

Problem solved  .

Thanks.

2,762 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi,

Could you please provide the terminal log for this node? Please define the TRACE_APP as TRUE.

What is the return value that you are seeing?

The addr16 variable, that you have, should be 0x0000 if you are trying to send data to the coordinator.

Then, is the end device in sleep mode?

Regards,

Mario

2,762 Views
jun951753jun951
Contributor III

W%4DU8D_TXQSRB@C16HGA47.png

addr16= 0x0000;

I don't know if the node is dormant.

The end device can send data directly to the coordinator?No router in between

0 Kudos
Reply