How can I implement Connection Parameters Request Procedure on QN908x as Peripheral device?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can I implement Connection Parameters Request Procedure on QN908x as Peripheral device?

Jump to solution
4,612 Views
daisuke
Contributor II

Hello,

I would like to code "Connection Parameters Request Procedure" to QN908x as a peripheral role.  Has anyone already implemented this?

I was searching sample codes for this, but I could not find any (even though there are many other sample code for services/profiles).

If I could get any sample code/snippet for this, it would be much appreciated.

Thanks,

Daisuke  

1 Solution
4,277 Views
gerardo_rodriguez
NXP Employee
NXP Employee

Hello Daisuke,

You can use the Gap_UpdateConnectionParameters() API from the peripheral to issue a Connection Parameter Update Request, but it will depend on the master if it will accept or reject the request.

Example:

Gap_UpdateConnectionParameters(mPeerDeviceId, gGapDefaultMinConnectionInterval_d , gGapDefaultMaxConnectionInterval_d, gGapDefaultConnectionLatency_d, gGapDefaultSupervisionTimeout_d, gGapConnEventLengthMin_d, gGapConnEventLengthMax_d);‍‍

Regards,

View solution in original post

3 Replies
4,277 Views
gerardo_rodriguez
NXP Employee
NXP Employee

Hello Daisuke,

You can use the Gap_UpdateConnectionParameters() API from the peripheral to issue a Connection Parameter Update Request, but it will depend on the master if it will accept or reject the request.

Example:

Gap_UpdateConnectionParameters(mPeerDeviceId, gGapDefaultMinConnectionInterval_d , gGapDefaultMaxConnectionInterval_d, gGapDefaultConnectionLatency_d, gGapDefaultSupervisionTimeout_d, gGapConnEventLengthMin_d, gGapConnEventLengthMax_d);‍‍

Regards,

4,277 Views
joachimk
Contributor II

Where to call this function? Do you have example code?

0 Kudos
Reply
4,277 Views
daisuke
Contributor II

Hello Gerardo,

Thank you very much for your reply.

Now, My 9080 as peripheral can send connection parameter update request to the peer.

Best Regards,

Daisuke