GENFSK Programming Documentation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GENFSK Programming Documentation

1,310 Views
Brainiac
Contributor II

Hello,

I’m encountering difficulties implementing GENFSK mode on your MCU MCXW716.

The process isn’t intuitive, and I haven’t been able to find clear documentation on how to configure and program the radio module in GENFSK, nor which SDK components (GenFSK stack, drivers, utilities, etc.) are required for a minimal setup Could you please provide:

A step-by-step guide to initialize and control GENFSK (bitrate, CRC, preamble, packet configuration, callbacks).

A list of the necessary SDK modules and example projects for a basic GENFSK application.

Thank you very much for your help!

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,268 Views
sofiaurueta
NXP Employee
NXP Employee

Hello,

Hope you are doing well.

 

There are two documents that have all the related information to the GENFSK Link Layer as well as running the Connectivity Test demo application:

The "Generic FSK Link Layer Quick Start Guide.pdf" and the "Generic FSK Link Layer API Reference Manual.pdf".

 

I am checking about the availability of these documents, but you can refer to them on SDK v2.16.100 under the following path <installation path>\docs\wireless\GENFSK

 

Best Regards,

Ana Sofia.

0 Kudos
Reply