FRDM-KW38 using the internal flash method for integrating OTAP service

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-KW38 using the internal flash method for integrating OTAP service

5,404 Views
Lincoln
Contributor III

Hi,

When working on integrating OTAP client service into a BLE central device, I meet a problem for using the internal flash storage method. 

I import the AN12980SW sample and follow the same setting process in the attached document including the project settings and the storage configurations. (the diagrams below are my settings.)

Lincoln_0-1640830865072.png

Lincoln_1-1640830893746.png

After clean and then build the project, the errors below show up.

Lincoln_2-1640831184818.png

How can I to deal with it?

 

Thank you for your help!

Labels (1)
0 Kudos
Reply
5 Replies

5,338 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @Lincoln,

Just to confirm, are you trying to update the Central device using OTA?

Did you follow the steps in the next community post?

Configuring and Programming OTAP Client Software in MCUXpresso IDE

Regards,

Mario

 

0 Kudos
Reply

5,324 Views
Lincoln
Contributor III

Hi @mario_castaneda,

Just to confirm, are you trying to update the Central device using OTA? Yes.

Did you follow the steps in the next community post? Yes, I did.

I attached the project which I import from AN12980SW and only modify the settings I've mentioned above for internal flash configuration.

 

note:

I am working with SDK version 2.6.14.

5,302 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @Lincoln,

I am not sure if I am following. Did you import and compile the project before any modification?

Are you following this chapter?

5.3 Creating a Temp Coll S-Record image to update the software

Regards,

Mario

0 Kudos
Reply

5,294 Views
Lincoln
Contributor III

Hi @mario_castaneda,

I am stuck on this chapter :

5.2 Creating a Temp Coll - OTAP S - record image to update the software

 

After import the Temp Coll-OTAP demo in my IDE, I modify its storage configurations for internal flash storage because the default is setting to external flash storage.

Before clean and build the project, I remove the FILL and BYTE statements in end_text.ldt linker script.

The errors show up as I have mentioned above, thus S-Record file cannot be generated.

0 Kudos
Reply

5,276 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @Lincoln,

The issue is expected because the program flash is using approx 270KB of memory, o it is more than 50% of the memory, and the internal storage for the new image will need a similar size.

mario_castaneda_0-1641415556347.png

You have 2 options.

-Reduce the code and be sure that it will not exceed the 244 KB

-Use the external memory

Regards,

Mario

 

0 Kudos
Reply