FRDM-KW24D512 with raspberry pi

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-KW24D512 with raspberry pi

1,830件の閲覧回数
waynezhao
Contributor I

I have made FRDM-KW24D512 work with iMX Ultralight linux board. The FRDM-KW24D512 was plugged in the Arduino connector in the iMXUl6 board and they work as Thread border gateway. Eveything works.

Now I want to make the FRDM-KW24D512 to work with raspberry pi. According to the documentation, the connection

between the FRDM-24D512 and any linux host need to be UART.  I have connect the UART of both. However

the firmware(thread_host_controller_device_imx6ulevk) ) in FDRM-25D512 is not running properly.  Should I connect some more wires between the FRDM-24D512 and the raspberry pi besides UART?

ラベル(1)
0 件の賞賛
返信
0 返答(返信)