Device information is removed from PDM when Device is already joined

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Device information is removed from PDM when Device is already joined

1,696件の閲覧回数
vihang_jani
Contributor I

Hi NXP Team, 

[IT'S CRITICAL ISSUE]


I am facing issue when Device(sprint#10 SDK) is already joined then update device firmware with sprint#12 over sprint#10. 

After that NCP PDM data is erased. I don't konw how is doing without call any PDM erase related API. 

Please provide Root Cause and Any dependency is there in sprint#10 or #12? 

For your Reference :

SmartEnergy Sprint#10 : 
HOST Version : JN-SW-4364-ZigBee-SmartEnergy1.x-v1721 
NCP Version : JN-SW-4170-v1719 

SmartEnergy Sprint#12 : 
HOST Version : JN-SW-4364-ZigBee-SmartEnergy1.x-v1779 
NCP version : JN-SW-4170-v1773 

PFA Log file. 

I hope you can catch up my query on the highest and reply me as soon as possible.

ラベル(1)
0 件の賞賛
返信
1 返信

1,563件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Vihang,

Could you please provide the SW and AN that you are working on?

We do not provide this SW. JN-SW-4364-ZigBee-SmartEnergy1.x-v1721

Regards,

Mario

0 件の賞賛
返信