Determining ZB PRO Network to Join Based on LQI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Determining ZB PRO Network to Join Based on LQI

2,875 次查看
ptaylor
Contributor I

The ZigBee PRO Stack User Guide (JN-UG-3101) suggests that an application can determine the network to connect to (from a list of networks obtained with a Network Discovery) based on the LQI. However, the network discovery complete event structure does not include any direct or indirect LQI value for the discovered networks. Is there a relatively simple way to accomplish this functionality (connect to network with highest LQI value)?

pastedImage_1.png

标签 (1)
标记 (2)
0 项奖励
回复
3 回复数

2,697 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Peter,

The beacon filtering is enabled using API ZPS_bAppAddBeaconFilter in Base device application code in bdb_start.c as below:

PUBLIC void BDB_vSetAssociationFilter()
{
   sBeaconFilter.pu64ExtendPanIdList = NULL;
   sBeaconFilter.u8ListSize = 0;
   sBeaconFilter.u8Lqi = BEACON_FILTER_LQI_VALUE;

   switch(ZPS_eAplZdoGetDeviceType())
   {
     case ZPS_ZDO_DEVICE_ENDDEVICE:
        sBeaconFilter.u16FilterMap =  BF_BITMAP_CAP_ENDDEVICE | \
                                      BF_BITMAP_PERMIT_JOIN |\
                                      BF_BITMAP_LQI;
          break;
     case ZPS_ZDO_DEVICE_ROUTER:
        sBeaconFilter.u16FilterMap =  BF_BITMAP_CAP_ROUTER | \
                                      BF_BITMAP_PERMIT_JOIN |\
                                      BF_BITMAP_LQI;
          break;
     default:
        //impossible!
          break;
    }
     ZPS_bAppAddBeaconFilter(&sBeaconFilter);
}‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

 

The parameters for beacon filtering are explained in details in section  7.2.3.5 tsBeaconFilterType of JN-UG-3113 and description for LQI is as below:

 

u8Lqi is the minimum LQI value (in the range 0 to 255) of an acceptable beacon (any beacon with LQI value less than this minimum will be filtered out) - if required, this field must be enabled through bit 2 in the u8FilterMap bitmap. So, this means 

 

So, if you set BEACON_FILTER_LQI_VALUE to 0 , this means the device will reject any beacon which has an LQI value less than 0 which means it shall accept all the beacons irrespective of LQI value as the range of LQI is 0 to 255.

Regards,

Mario

0 项奖励
回复

2,697 次查看
ptaylor
Contributor I

Mario, thank you for your response.

The Beacon filtering is the only possible solution I could see as well. However, this is a bit of a hack for being able to select the network with the best LQI. You would have to complete multiple Network Discovery scans with a lower LQI filter on each successive scan until you found a network. It seems counter-intuitive that the LQI of each discovered network is not included in the ZPS_EVENT NWK_DISCOVERY_COMPLETE structure. I assume the stack has the value, it's just not passed along with the event structure.

All that being said, I do understand that LQI is probably typically one of the last considerations when choosing a network to join and the Beacon Filter is probably sufficient for TouchLink-type Network Discovery.

0 项奖励
回复

2,697 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Peter,

You are right the LQI is not the first consideration when the device is choosing a network. As you know, that value is not constant and could be affected by the walls, temperature, humidity, etc...

Please let me know if you have any further question.

Regards,

Mario

0 项奖励
回复