Create A new KW37 Project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Create A new KW37 Project

Jump to solution
1,874 Views
JackYu2
Contributor I
I have a MKW37A512 board. I run kw38 project In the board. It CAN NOT work. But I CAN NOT find any project about KW37 in NXP website. How can I Get the KW37 demo projct??
0 Kudos
Reply
1 Solution
1,856 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. If you would like to test some examples, you would need to select the FRDM-KW38 in the MCUXpresso SDK Builder.

Also, you would need to use the MKW37 SDK to be able to adequate the FRDM example to the KW37 memories.

 

Hope this helps!

 

Regards,

Ricardo

View solution in original post

0 Kudos
Reply
1 Reply
1,857 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. If you would like to test some examples, you would need to select the FRDM-KW38 in the MCUXpresso SDK Builder.

Also, you would need to use the MKW37 SDK to be able to adequate the FRDM example to the KW37 memories.

 

Hope this helps!

 

Regards,

Ricardo

0 Kudos
Reply