Clarification Required on EPC and User Memory Specifications

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Clarification Required on EPC and User Memory Specifications

1,816 Views
kalyanperika
Contributor I

I am currently working on the development of an RFID tag, including the design of the microchip, antenna, and enclosure. At this stage, I need a suitable microchip to incorporate into the tag.

Here are the specifications I require for the microchip:

  • EPC Memory: 224 bits
  • User Memory: 3kbit
  • Kill Password: 32 bits
  • Read Range: 14 - 16 meters (On metal)
  • Operational Frequency: 865 – 868 MHz or 902 – 928 MHz

Could you kindly provide a microchip that meets these specifications? Your prompt assistance in supplying this component would be greatly appreciated.
I shared on datasheet which is reverse to my specifications once go through that and let me know is that datasheet is enough

Looking forward to your response.

Best regards,
perika kalyan

0 Kudos
Reply
0 Replies