Can zigbee experts give me some advice?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can zigbee experts give me some advice?

2,377件の閲覧回数
yjvijfhvk
Contributor I

Dear friends,
I am a newcomer to the development of ZIGBEE, I should first look at what documents are better, and the software developed is downloaded there.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,272件の閲覧回数
patrick_pan
NXP Employee
NXP Employee

Hi, Liu

What kind of HW you will used for Zigbee development ? 

if you want to use KW , then you will use MCUXpresso to build App;

if you want to use JN , then you should use BeyondStudio for compiling 

0 件の賞賛
返信

2,272件の閲覧回数
yjvijfhvk
Contributor I
0 件の賞賛
返信

2,272件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Liu,

Do you plan to use KW or JN for your application?, depending of this choise, I would suggest to check the SDK (KW) or the examples for the JN, in each of this package code there's some documentation you can check and some demo examples.

If you want to download the SDK, please check the following link and in the search bar, browse KW41Z:

Welcome | MCUXpresso SDK Builder 

For the examples, in the webpage you mention, please download first beyond studio. Also download the JN - AN - 1220 and  JN - AN - 1216, the first is an example for a sensor and the second is the control bridge that control the first one. This is a good example to start.

I hope this helps you.

 

Best Regards,

Alexis Andalon

0 件の賞賛
返信