CLRC663 - ISO 18000

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CLRC663 - ISO 18000

2,920件の閲覧回数
jmunoa
Contributor I

Hello,

I just acquired a 13.56 MHz multiprotocol reader, CLRC663 red board, in order to communicate with SL2S1512FTB tags, that support  ISO/IEC 18000-3 mode 3/EPC Class-1 HF.

The tools available in NXP site include a script based software "RC663 Serial RS 232 Test Program" and some script examples for different protocols such as ISO15693, ISO14443.. but I can't find any script to test this ISO 18000-3.

Does someone know where can I find any scripts for that software that configures the reader in ISO18000 mode?

Thank you very much.

Best regards,

Jon

0 件の賞賛
返信
1 返信

2,522件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Jon Munoa:

Thank you for using our NFC  community.

You are right the package unfortunately does not include a script for ICODE tags. There are some examples for ICODE using the CLEV663B blue board together with the NFC Reader Library, under the "Software and Tools" tab in the product page:

High performance NFC reader solution|NXP

Regards!

Jorge Gonzalez

0 件の賞賛
返信