BeeStack5.0.0 soucres

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BeeStack5.0.0 soucres

1,607件の閲覧回数
grzegorzskiba
Contributor I

Hello, 

Is it possible to get BeeStack5.0.0 sources ? We are working on porting our application from IAR to KDS IDE. In example applications precompiled library (BeeStackZrRsRNPSp2_M4.a) is used which was compiled with IAR compiler. Is it possible to get BeeStackZrRsRNPSp2_M4.a soucres in order to recompile BeeStackZrRsRNPSp2_M4.a library with GCC compiler ?  

Regards Grzegorz

ラベル(2)
0 件の賞賛
返信
1 返信

1,450件の閲覧回数
jc_pacheco
NXP Employee
NXP Employee

Hello Grzegorz, unfortunately those sources are not shared outside of NXP.

0 件の賞賛
返信