BeeAppInit main() doesnt stop at InterruptInit() because it is not defined anywhere. Also missing ApsManagementService.c and SspNwkKeyMgmt.c

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BeeAppInit main() doesnt stop at InterruptInit() because it is not defined anywhere. Also missing ApsManagementService.c and SspNwkKeyMgmt.c

Jump to solution
3,105 Views
atillametetured
Contributor V

Here is the logfile;

Wed Feb 01, 2017 09:41:14: IAR Embedded Workbench 7.80.3 (armproc.dll)
Wed Feb 01, 2017 09:41:14: Loaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.5\arm\config\debugger\NXP\Kxx.dmac
Wed Feb 01, 2017 09:41:14: Loaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.5\arm\config\debugger\NXP\KW2xD_Trace.dmac
Wed Feb 01, 2017 09:41:15: JLINK command: ProjectFile = D:\Users\aturedi\Desktop\Smart Home Gateway Services\BeeKitSolutions\SGCA\HomeGateway\Ha HomeGateway\settings\Ha HomeGateway_Release.jlink, return = 0
Wed Feb 01, 2017 09:41:15: Device "MKW24D512XXX5" selected.
Wed Feb 01, 2017 09:41:15: DLL version: V6.12f, compiled Jan 13 2017 16:37:50
Wed Feb 01, 2017 09:41:15: Firmware: J-Link V10 compiled Jan 9 2017 17:48:51
Wed Feb 01, 2017 09:41:15: JTAG speed is initially set to: 32 kHz
Wed Feb 01, 2017 09:41:15: TotalIRLen = 4, IRPrint = 0x01
Wed Feb 01, 2017 09:41:15: TotalIRLen = 4, IRPrint = 0x01
Wed Feb 01, 2017 09:41:15: AP-IDR: 0x24770011, Type: AHB-AP
Wed Feb 01, 2017 09:41:15: AHB-AP ROM: 0xE00FF000 (Base addr. of first ROM table)
Wed Feb 01, 2017 09:41:15: Found Cortex-M4 r0p1, Little endian.
Wed Feb 01, 2017 09:41:15: FPUnit: 6 code (BP) slots and 2 literal slots
Wed Feb 01, 2017 09:41:15: CoreSight components:
Wed Feb 01, 2017 09:41:15: ROMTbl 0 @ E00FF000
Wed Feb 01, 2017 09:41:15: ROMTbl 0 [0]: FFF0F000, CID: B105E00D, PID: 000BB000 SCS
Wed Feb 01, 2017 09:41:15: ROMTbl 0 [1]: FFF02000, CID: B105E00D, PID: 003BB002 DWT
Wed Feb 01, 2017 09:41:15: ROMTbl 0 [2]: FFF03000, CID: B105E00D, PID: 002BB003 FPB
Wed Feb 01, 2017 09:41:15: ROMTbl 0 [3]: FFF01000, CID: B105E00D, PID: 003BB001 ITM
Wed Feb 01, 2017 09:41:15: ROMTbl 0 [4]: FFF41000, CID: B105900D, PID: 000BB9A1 TPIU
Wed Feb 01, 2017 09:41:15: ROMTbl 0 [5]: FFF42000, CID: B105900D, PID: 000BB925 ETM
Wed Feb 01, 2017 09:41:16: Hardware reset with strategy 0 was performed
Wed Feb 01, 2017 09:41:16: Initial reset was performed
Wed Feb 01, 2017 09:41:16: Found 1 JTAG device, Total IRLen = 4:
Wed Feb 01, 2017 09:41:16: #0 Id: 0x4BA00477, IRLen: 4, IRPrint: 0x1 CoreSight JTAG-DP
Wed Feb 01, 2017 09:41:16: 3196 bytes downloaded and verified (40.01 Kbytes/sec)
Wed Feb 01, 2017 09:41:16: Loaded debugee: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.5\arm\config\flashloader\NXP\FlashK60Dxxx64K.out
Wed Feb 01, 2017 09:41:16: Target reset
Wed Feb 01, 2017 09:41:18: Downloaded D:\Users\aturedi\Desktop\Smart Home Gateway Services\BeeKitSolutions\SGCA\HomeGateway\Ha HomeGateway\Release\Exe\Ha HomeGateway.out to flash memory.
Wed Feb 01, 2017 09:41:18: Hardware reset with strategy 0 was performed
Wed Feb 01, 2017 09:41:20: 99012 bytes downloaded into FLASH and verified (28.69 Kbytes/sec)
Wed Feb 01, 2017 09:41:20: Loaded debugee: D:\Users\aturedi\Desktop\Smart Home Gateway Services\BeeKitSolutions\SGCA\HomeGateway\Ha HomeGateway\Release\Exe\Ha HomeGateway.out
Wed Feb 01, 2017 09:41:20: Hardware reset with strategy 0 was performed
Wed Feb 01, 2017 09:41:20: Target reset

Regards,

Mete

0 Kudos
Reply
1 Solution
2,908 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Atilla,

What is the beekit version that you are using?

Did you download the Beekit 3.0.2?

BeeKit Wireless Connectivity Toolkit|NXP 

Best Regards,

Mario

View solution in original post

3 Replies
2,909 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Atilla,

What is the beekit version that you are using?

Did you download the Beekit 3.0.2?

BeeKit Wireless Connectivity Toolkit|NXP 

Best Regards,

Mario

2,908 Views
atillametetured
Contributor V

Hi Mario,

It did not give me any run-time problems so I moved on with it.

Best Regards,

Mete

0 Kudos
Reply
2,908 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Atilla,

I'm sorry, I confused the last stack that we have.

Please take a look The Kinetis BeeStack ZigBee Protocol Stack (REV 5.0.0)

Search Results: beestack 5 

Hope it helps,

Mario

0 Kudos
Reply