BLE KW41Z Connection issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BLE KW41Z Connection issue

4,861件の閲覧回数
kevin_lang
Contributor II

Hello,

Is there a good example for KW41Z with 2 concurrent connections. 

I did one and when testing with mobile applications (did by a 3rd contractor), the 1st App connecting okay , while 2nd app (both Android and iOS) connected and then quickly KW41Z firmware received a Disconnection event. 

Mobile developer said he didn't initiate  disconnection, I also didn't call any API to disconnect, how could it happen?

Thanks you all in advance

Kevin

ラベル(2)
3 返答(返信)

4,709件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

Could you please try the wireless uart example with the IOT Toolbox? Does it work for you? 

Regards, 

Estephania 

0 件の賞賛
返信

4,709件の閲覧回数
kevin_lang
Contributor II

 Hello Estephania

Thank you! Yes, I use the wireless uart example and modified based on it , with the IOT Toolbox ,two connections is okay, but sometimes second connection status is always in Service Discovery (mAppServiceDisc_c), what can I do to  make it in mAppRunning_c ?

=================================

typedef enum appState_tag
{
mAppIdle_c,
mAppExchangeMtu_c,
mAppServiceDisc_c,
mAppRunning_c
} appState_t;

Best regards,

Kevin lang

0 件の賞賛
返信

4,707件の閲覧回数
miguel_reyes
NXP Employee
NXP Employee

Hi [email protected]‌, 

Here you can find attached a document lab that explains how to add a second connection to the heart rate sensor application. 

Hope this helps. 

Best regards,

Miguel