BLE Audio application support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BLE Audio application support

ソリューションへジャンプ
5,302件の閲覧回数
pavan252
Contributor II

Hello team,

My customer is looking for LE Audio streaming and Voice over Bluetooth with add-on sensors .

Currently i am using QN9080 for my sensor application but now i need to add LE audio application on top of this. Could you please advise if our QN9080 supports LE audio or is there any NXP BLE device which supports my application?

Thanks in advance.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
5,297件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

Our NXH series product may meet your needs.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

3 返答(返信)
5,297件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

Our NXH series product may meet your needs.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

5,271件の閲覧回数
pavan252
Contributor II

Hi 

Thanks for your reply.

After checking the datasheet of NXH series i have below query

Can i use NXH3670 for multiple one to one connections simultaneously? 

Because my Bluetooth device requires 

1. BLE audio playback application from mobile and

2. Simultaneously it has to share the data from sensors connected to it to another slave device.

Can i use NXH for this application or do i need to use piconet or mesh applications?

Please suggest.

 

Regards

Pavan.

0 件の賞賛
返信
5,221件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

Unfortunately, it can't.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信