BGU8052

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BGU8052

1,665件の閲覧回数
869019315
Contributor I

Can BGU8052 be used at 1.2ghz?How does 0IP3 and Gain change?

タグ(1)
0 件の賞賛
返信
1 返信

1,608件の閲覧回数
LPP
NXP Employee
NXP Employee

Please refer to this application note:
https://www.nxp.com/docs/en/application-note/AN11902.pdf

It provides the measurement results that have been carried out on the standard 1900MHz BGU8052 evaluation boards at 1.3GHz.


The measured IP3O is 35dBm. This value fits the datasheet spec (IP3O>32dBm) at 1900MH. We do not expect noticeable difference at 1.2GHz.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信