BGU7045 - switch time

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

BGU7045 - switch time

1,500 次查看
ricardopereira
Contributor I

Hi, 

There is no information on the datasheet about how fast does the BGU7045 switch between 14dB Gain mode to Bypass mode. Can you provide it please? 

Thank you for your time,

0 项奖励
回复
1 回复

1,417 次查看
LPP
NXP Employee
NXP Employee

NXP does not specify switch time but our RF application engineer measured it as following:

By using 3V at control line (pin 4) then the on time is 12us and the off (bypass) time is 19us .
Lowering the control voltage will lead to increase the switch time!


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复