Arrays and Structures support in ZCL (ZigBee)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Arrays and Structures support in ZCL (ZigBee)

2,006件の閲覧回数
bogdan_kostiv
Contributor I

Hi,

I'm working on a ZigBee solution where custom clusters will be used. In some clusters I would like to use arrays (E_ZCL_ARRAY = 0x48) and structures (E_ZCL_STRUCT = 0x4c). But as I see proper implementation of mentioned data types is missing. I'm wondering if there are plans to add support of arrays and structures to the ZCL.

BR,

Bogdan

ラベル(3)
0 件の賞賛
返信
1 返信

1,919件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Bodgan,

Unfortunately, right now, we do not have any implementation with the array or struct to the ZCL. We are working on a maintenance release for the Zigbee Stack. It is a good implementation but we do not have any plans for supporting this feature.

Regards,

Mario

0 件の賞賛
返信