Add a zone to IAS device command

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Add a zone to IAS device command

1,499件の閲覧回数
rostislav
Contributor III

I created a IAS ZED using Freescale beekit V 3.0.2 To make it operational I need adding a zone with IASZone_AddEntryInClientTable command (Group 0x70 Opcode 0x7E).

Unfortunatelu I couldn't find such command neither in BlackBox document  BSBBZTCRM Rev. 1.4 10/2013 nor in Command Console command list of Freescale Test tool 12 V 12.4.0.

Does exist an updated document? If it is presented in Freescale Test tool 12 V 12.4.0 then which name is used for the command?

0 件の賞賛
返信
0 返答(返信)