Activating Hotspot/AP 88W8997 with Android 11

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Activating Hotspot/AP 88W8997 with Android 11

1,587件の閲覧回数
rahmanuh
Contributor III

Hello,

While integrating Android HAL for Android 11 with 88W8997 PCIE-USB driver. I cannot activate the Hotspot. The STA works fine though.

Whenever I try to enable the AP/Hotspot via Android GUI, the kernel give this messages. And the AP cannot be activated. Could anyone give some hints to solve this?

evk_8mq:/ # [ 59.607447] init: starting service 'hostapd'...
[ 59.619464] init: Control message: Processed ctl.interface_start for '
[email protected]::IHostapd/default' from pid: 237 (/system/bin/hwservicemanager)
[ 59.739979] capability: warning: `hostapd' uses 32-bit capabilities (legacy support in use)
[59.819150] type=1400 audit(1627913138.799:49): avc: denied { sys_module } for comm="
[email protected]" capability=16 scontext=u:r:hal_wifi_default:s0 tcontext=u:r:hal_wifi_default:s0 tclass=capability permissive=0 evk_8mq:/ #
[ 64.607637] type=1400 audit(1627913143.587:50): avc: denied { sys_module } for comm="
[email protected]" capability=16 scontext=u:r:hal_wifi_default:s0 tcontext=u:r:hal_wifi_default:s0 tclass=capability permissive=0 evk_8mq:/ #
[ 66.156767] type=1400 audit(1627913145.135:51): avc: denied { sys_module } for comm="
[email protected]" capability=16 scontext=u:r:hal_wifi_default:s0 tcontext=u:r:hal_wifi_default:s0 tclass=capability permissive=0

Best regards,
Rahmanu

Edit: formating

0 件の賞賛
返信
0 返答(返信)