88W8801(LILY W131) WiFI SDIO chip - not responding after FW download

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

88W8801(LILY W131) WiFI SDIO chip - not responding after FW download

Jump to solution
880 Views
luqtd
Contributor II

Hello, I am trying to run the 88W8801 on an Nvidia AGX Orin, but unfortunately, I'm experiencing issues with a lack of response after fw_download. Any idea why this might be happening?

 

 

[  392.618241] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[  392.618541] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[  392.619180] cfg80211: loaded regulatory.db is malformed or signature is missing/invalid
[  392.629162] wlan: Loading MWLAN driver
[  392.631120] wlan: Register to Bus Driver...
[  392.632317] vendor=0x02DF device=0x9139 class=0 function=1
[  392.632408] Attach moal handle ops, card interface type: 0x10a
[  392.632582] SD8801: init module param from usr cfg
[  392.632605] card_type: SD8801, config block: 0
[  392.632608] cfg80211_wext=0xf
[  392.632611] cal_data_cfg=none
[  392.632612] ps_mode = 1
[  392.632614] fw_name=nxp/new.bin
[  392.632622] SDIO: max_segs=128 max_seg_size=65535
[  392.632625] rx_work=1 cpu_num=12
[  392.632640] Attach mlan adapter operations.card_type is 0x10a.
[  392.633036] wlan: Enable TX SG mode
[  392.633038] wlan: Enable RX SG mode
[  392.637804] Request firmware: nxp/new.bin
[  392.638422] WLAN FW already running! Skip FW download
[  392.638470] WLAN FW is active
[  392.638472] on_time is 392636776160
[  397.790492] Timeout cmd id (397.788783) = 0xa9, act = 0x0
...
...
...


[  397.795899] mp_wr_bitmap: 0x0 mp_wr_ports=0x0 len=0 curr_wr_port=0x0
..
..
..
[  397.796170] mp_wr_bitmap: 0x0 mp_wr_ports=0x0 len=0 curr_wr_port=0x0
[  397.796196] 0x00 
[  397.796228] 0x00 
[  397.796248] 0x00 
[  397.796280] 0x00 
[  397.796298] 0x00 
[  397.796316] 0x00 
[  397.796345] 0x00 
[  397.796363] 0x00 

[  397.796428] bss_index = 0, tx_pkts_queued = 0
[  397.796468] -------- Dump info End---------
[  397.799854] SDIO Func0 (0x0-0x9): 32 02 02 02 03 00 00 02 03 00 
[  397.800053] SDIO Func1 (0x10-0x17): 00 00 00 00 00 00 00 00 
[  397.800165] SDIO Func1: (0x28) 00 (0x30) 08 (0x34) 07 (0x38) 10 (0x3c) 00 
[  397.800415] SDIO Func1 (0x60-0x6a): dc fe 1c 00 67 01 03 01 03 00 30 
[  397.902354] SDIO Func1 (0x60-0x6a): dc fe 26 00 71 01 03 01 03 00 30 
[  397.902442] woal_request_fw failed
[  397.902446] Firmware Init Failed
[  397.907748] Free module params
[  397.907760] woal_add_card failed
[  397.907825] wlan_sdio: probe of mmc1:0001:1 failed with error -1
[  397.908292] wlan: Register to Bus Driver Done
[  397.908297] wlan: Driver loaded successfully

 

 

0 Kudos
Reply
1 Solution
756 Views
luqtd
Contributor II

I'm not entirely sure why, but removing the no-sd property and changing the bus-width from 4 to 1 in the device tree seems to have resolved the issue. I’ll investigate this further and will post updates here on what I find.

Interestingly, after the first firmware download, it started working even with the original device tree configuration. Really strange behavior.

View solution in original post

0 Kudos
Reply
10 Replies
840 Views
luqtd
Contributor II
[  121.555042] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[  121.555414] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[  121.556033] cfg80211: loaded regulatory.db is malformed or signature is missing/invalid
[  121.567292] wlan: Loading MWLAN driver
[  121.568170] wlan: Register to Bus Driver...
[  121.569339] vendor=0x02DF device=0x9139 class=0 function=1
[  121.569450] Attach moal handle ops, card interface type: 0x10a
[  121.569454] No module param cfg file specified
[  121.569457] SDIO: max_segs=128 max_seg_size=65535
[  121.569459] rx_work=1 cpu_num=12
[  121.569476] Attach mlan adapter operations.card_type is 0x10a.
[  121.569896] wlan: Enable TX SG mode
[  121.569898] wlan: Enable RX SG mode
[  121.571461] Request firmware: nxp/sd8801_uapsta.bin
[  121.572044] WLAN FW already running! Skip FW download
[  121.572113] WLAN FW is active
[  121.572116] on_time is 121568811104
[  121.572640] get fw info failed! status=-1, error_code=0x0
[  121.572644] woal_init_priv: get_fw_info failed 
[  121.573011] Register NXP 802.11 Adapter mlan0
[  121.573015] get fw info failed! status=-1, error_code=0x0
[  121.573017] woal_add_interface: get_fw_info failed 
[  121.619528] Failed to add interface
[  121.651405] woal_request_fw failed
[  121.651412] Firmware Init Failed
[  121.660746] Free module params
[  121.660769] woal_add_card failed
[  121.660867] wlan_sdio: probe of mmc1:0001:1 failed with error -1
[  121.661267] wlan: Register to Bus Driver Done
[  121.661275] wlan: Driver loaded successfully

When i remove the module with "modprobe -r moal" and probe it again. I am getting also logs like this. 

0 Kudos
Reply
836 Views
luqtd
Contributor II
modprobe moal req_fw_nowait=1

 

..
..
[  474.021924] wlan: Enable RX SG mode
[  474.023468] Request firmware: nxp/sd8801_uapsta.bin
[  474.023650] wlan: Register to Bus Driver Done
[  474.023652] wlan: Driver loaded successfully
[  474.025714] WLAN FW already running! Skip FW download
[  474.025780] WLAN FW is active
[  474.025782] on_time is 474022476992
[  479.199409] Timeout cmd id (479.196095) = 0xa9, act = 0x0
[  479.199623] a9 
[  479.199652] 00 
[  479.199673] 08 
[  479.199691] 00 
[  479.199710] 01 
[  479.199729] 00 
[  479.199747] 00 
[  479.199767] 00 
[  479.199786] 00 
[  479.199805] 00 
[  479.199823] 00 
[  479.199842] 00 
[  479.199860] 00 
[  479.199879] 00 
[  479.199898] 00 
[  479.199916] 00 

[  479.199957] BSS type = 0 BSS role= 0
[  479.199988] ------------Dump info-----------
[  479.200017] Commmand Timeout
[  479.200050] pending command id: 0x242 ioctl_buf=0000000000000000
[  479.200081] pending command id: 0x3 ioctl_buf=0000000000000000
[  479.200099] No pending scan command
[  479.200122] mlan_processing =0
[  479.200147] main_lock_flag =0
[  479.200171] main_process_cnt =1
[  479.200195] delay_task_flag =0
[  479.200216] mlan_rx_processing =0
[  479.200239] rx_pkts_queued=0
[  479.200261] more_task_flag = 0
[  479.200286] num_cmd_timeout = 1
[  479.200307] last_cmd_index = 1
[  479.200327] last_cmd_id = 
[  479.200349] 0x0 

.
.
[  479.201631] num_data_h2c_failure = 0
[  479.201651] num_cmd_h2c_failure = 0
[  479.201677] num_data_c2h_failure = 0
[  479.201707] num_cmdevt_c2h_failure = 0
[  479.201728] num_int_read_failure = 0
[  479.201752] last_int_status = 0
[  479.201783] num_alloc_buffer_failure = 0
[  479.201814] num_pkt_dropped = 0
[  479.201833] num_no_cmd_node = 0
[  479.201854] num_event_deauth = 0
[  479.201872] num_event_disassoc = 0
[  479.201911] num_event_link_lost = 0
[  479.201933] num_cmd_deauth = 0
[  479.201950] num_cmd_assoc_success = 0
[  479.201974] num_cmd_assoc_failure = 0
[  479.202005] num_cons_assoc_failure = 0
[  479.202026] cmd_resp_received=0
[  479.202044] event_received=0
[  479.202065] max_tx_buf_size=2048
[  479.202097] tx_buf_size=2048
[  479.202118] curr_tx_buf_size=2048
[  479.202142] data_sent=1 cmd_sent=1
[  479.202164] ps_mode=1 ps_state=0
[  479.202193] wakeup_dev_req=0 wakeup_tries=0 wakeup_timeout=0
[  479.202217] hs_configured=0 hs_activated=0
[  479.202240] pps_uapsd_mode=0 sleep_pd=0
[  479.202279] tx_lock_flag = 0
[  479.202299] scan_processing = 0
[  479.202318] scan_state = 0x0
[  479.202339] bypass_pkt_count=0
[  479.202371] mp_rd_bitmap=0x0 curr_rd_port=0x1
[  479.202395] mp_wr_bitmap=0x0 curr_wr_port=0x1
[  479.202414] mp_data_port_mask = 0xfffe
[  479.202441] last_recv_rd_bitmap=0x0 mp_invalid_update=0
[  479.202475] last_recv_wr_bitmap=0x0 last_mp_index=0
[  479.202501] mp_wr_bitmap: 0x0 mp_wr_ports=0x0 len=0 curr_wr_port=0x0
.
.
.
[  479.204759] 0x00 
[  479.204776] 0x00 
[  479.204798] 0x00 

[  479.204857] mp_wr_bitmap: 0x0 mp_wr_ports=0x0 len=0 curr_wr_port=0x0
[  479.204892] 0x00 
[  479.204910] 0x00 
[  479.204928] 0x00 
[  479.204959] 0x00 
[  479.204991] 0x00 
[  479.205010] 0x00 
[  479.205027] 0x00 
[  479.205045] 0x00 

[  479.205108] bss_index = 0, tx_pkts_queued = 0
[  479.205134] -------- Dump info End---------
[  479.211648] SDIO Func0 (0x0-0x9): 32 02 02 02 03 00 00 02 03 00 
[  479.212488] SDIO Func1 (0x10-0x17): 00 00 00 00 00 00 00 00 
[  479.213010] SDIO Func1: (0x28) 00 (0x30) 08 (0x34) 07 (0x38) 10 (0x3c) 00 
[  479.214100] SDIO Func1 (0x60-0x6a): dc fe 19 00 2e 01 03 01 06 00 30 
[  479.319160] SDIO Func1 (0x60-0x6a): dc fe 24 00 38 01 03 01 06 00 30 
[  479.319185] woal_request_fw_dpc failed
0 Kudos
Reply
821 Views
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

I just did a test using an iMX8MP running Linux 5.15.71 and a 2DS wireless module and seems to be working on my side.

root@imx8mpevk:~# uname -r
5.15.71+g50912be38601
root@imx8mpevk:~# modprobe moal mod_para=nxp/wifi_mod_para.conf
[   29.718678] mlan: loading out-of-tree module taints kernel.
[   29.743284] wlan: Loading MWLAN driver
[   29.747330] wlan: Register to Bus Driver...
[   29.758102] vendor=0x02DF device=0x9139 class=0 function=1
[   29.763683] Attach moal handle ops, card interface type: 0x10a
[   29.770597] SD8801: init module param from usr cfg
[   29.775450] card_type: SD8801, config block: 0
[   29.779910] cfg80211_wext=0xf
[   29.782888] max_vir_bss=1
[   29.785511] cal_data_cfg=none
[   29.788488] ps_mode = 1
[   29.790945] auto_ds = 1
[   29.793396] host_mlme=enable
[   29.796305] fw_name=nxp/sd8801_uapsta.bin
[   29.800344] SDIO: max_segs=128 max_seg_size=65535
[   29.805061] rx_work=1 cpu_num=4
[   29.808227] Attach mlan adapter operations.card_type is 0x10a.
[   29.815228] wlan: Enable TX SG mode
[   29.818755] wlan: Enable RX SG mode
[   29.829669] Request firmware: nxp/sd8801_uapsta.bin
[   30.114525] Wlan: FW download over, firmwarelen=256744 downloaded 256744
[   30.317972] WLAN FW is active
[   30.320953] on_time is 30319390625
[   30.353278] fw_cap_info=0xba3, dev_cap_mask=0xffffffff
[   30.483665] Register NXP 802.11 Adapter mlan0
[   30.489778] Register NXP 802.11 Adapter uap0
[   30.499256] Register NXP 802.11 Adapter wfd0
[   30.505382] wlan: version = SD8801----14.92.36.p178-MM5X14366.p5-GPL-(FP92)
[   30.514305] wlan: Register to Bus Driver Done
[   30.518750] wlan: Driver loaded successfully
root@imx8mpevk:~# ifconfig mlan0 up

This is the configuration for 8801:

SD8801 = {
        cfg80211_wext=0xf
        max_vir_bss=1
        cal_data_cfg=none
        ps_mode=1
        auto_ds=1
        host_mlme=1
        fw_name=nxp/sd8801_uapsta.bin
}

Please let me know if you notice any difference.
Regards,

Daniel.

0 Kudos
Reply
795 Views
luqtd
Contributor II

If it’s not clock gating, do you have any idea why this might be happening?

0 Kudos
Reply
782 Views
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

I'm not entirely sure. 

Nevertheless, I notice the fw is not being downloaded to the SoC since you get a "WLAN FW already running! Skip FW download". Is there any step you execute before the logs you sent me?

Regards,

Daniel.

0 Kudos
Reply
757 Views
luqtd
Contributor II

I'm not entirely sure why, but removing the no-sd property and changing the bus-width from 4 to 1 in the device tree seems to have resolved the issue. I’ll investigate this further and will post updates here on what I find.

Interestingly, after the first firmware download, it started working even with the original device tree configuration. Really strange behavior.

0 Kudos
Reply
807 Views
luqtd
Contributor II

I think the main difference is that I’m using Nvidia’s board with a relatively newer kernel.

I’ve noticed that my Nvidia’s board uses Clock Gating. Do you think that could be causing the issue?

0 Kudos
Reply
859 Views
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

What OS version are you using?

What Driver and FW are you using?

Could you please share with me the whole terminal output of your test (commands)?

Regards,

Daniel.

0 Kudos
Reply
849 Views
luqtd
Contributor II

I am using a Linux OS based on Nvidia-Jetpack(v36.3) with kernel 5.15.136-l4t. I also tried it on kernel 5.10, but the result was the same.

Driver: github.com/nxp-imx/mwifiex.git - branch: lf-5.15.71_2.2.0

Firmware: github.com/NXP/imx-firmware.git - branch: lf-5.15.71_2.2.0

The command i use:

 

 

modprobe moal

 

 

I also tried but the result was the same

 

 

modprobe moal mfg_mode=1 cal_data_cfg=none drv_mode=1 fw_name=nxp/sd8801.bin

 

 

 

Thanks in advance for help!

 

 

0 Kudos
Reply
876 Views
luqtd
Contributor II

nxp/new.bin is a copy of nxp/sd8801_uapsta.bin

0 Kudos
Reply