why i cannot upgrade the PN5180's firmware?
[2022.01.27 20:01:33]:FATAL_ERROR:UcVcomBalDelegate:Timeout Error while writing to COM6
[2022.01.27 20:01:33]:ERROR:BoardConnectionViewModel:Secure Firmware Upgrade Failed. Status=BAL,IO_TIMEOUT
Solved! Go to Solution.
the bin file run in LPC1769 mcu is C:\nxp\NxpNfcCockpit_v6.3.0.0\ABENDToVCOM\fw\lpc_main.bin
and i can read the M1 card's UUID.
why i cannot upgrade the PN5180's firmware?
why i use C:\nxp\NxpNfcCockpit_v6.3.0.0\ABENDToVCOM\fw\lpc_main.bin file can read out M1's UUID,but i cannot operate type B/ISO15693/Felica card successful? why?
if i want use NXP NFC Cockpit v6.3.0.0 to operate type B/ISO15693/Felica card success,i must burn the C:\nxp\NxpNfcCockpit_v6.3.0.0\firmware\Secondary_PN5180\BootLoader_And_Nfcrdlib_SimplifiedAPI_EMVCo_Secondary.bin file to LPC1769 mcu?
Hi @andy_Musk
I did a quick check, programed BootLoader_And_Nfcrdlib_SimplifiedAPI_EMVCo_Secondary.bin into my PN5180 board with MCUXpresso IDE. From the cockpit, I can see type B is supported.
you are great!!!
now ,i can upgrade the PN5180's firmware!!! but i still cannot operate the Type B card.
I would suggest you create a new thread, since this thread is very long
ok!!!
C:\nxp\NxpNfcCockpit_v6.3.0.0\ABENDToVCOM\fw\lpc_main.bin vs
C:\nxp\NxpNfcCockpit_v6.3.0.0\firmware\Secondary_PN5180\BootLoader_And_Nfcrdlib_SimplifiedAPI_EMVCo_Secondary.bin
the two bin files arenot same? which is the difference? what is their order?
lpc_main.bin is for legacy ABEND driver.
my problem isnot be resolved!!!
please refer to below link for making Hex Files from binary files. but I would suggest you program bin file with MCUXpresso IDE
https://developer.arm.com/documentation/ka004226/latest
ok, i will try your way!!!
i can upgrade the PN5180 firmware use NXP NFC Cockpit v4.0.0.0.but the NXP NFC Cockpit v6.3.0.0 cannot work!!! why?
i can upgrade the PN5180 firmware use NXP NFC Cockpit v4.0.0.0.but the NXP NFC Cockpit v6.3.0.0 cannot work!!! why?
i have readed the AN11781.pdf for many times. but it cannot resolve my problem. the problem maybe the NXP NFC Cockpit v6.3.0.0 tool.but i cannot sure!
now i can use my pn5180 demo board to read M1 card with NXP NFC Cockpit v6.3.0.0 tool.but when i upgrade the PN5180's firmware.the NXP NFC Cockpit v6.3.0.0 tool print error log. i donot know why!!!
Hi
I would suggest you refer to AN11781 PN5180 Secure firmware update.
https://www.nxp.com/docs/en/application-note/AN11781.pdf
check the system requirements and hardware requirements.
Regards
Daniel
when i open the NXP NFC Cockpit v6.3.0.0 software. the above interface will show!!!
the bin file run in LPC1769 mcu is C:\nxp\NxpNfcCockpit_v6.3.0.0\ABENDToVCOM\fw\lpc_main.bin
the bin file use in LPC1769 mcu is right?
maybe my PN5180 chip version doesnot support firmware upgrade?
From your picture, your PNEV5180 PC driver is an older version, ABEND driver. This interface has been replaced with a VCOM interface, so the ABEND driver is not required any more. Please install VCOM driver manually. user manual is AN11744 PN5180 Evaluation board quick start guide.
Please refer to AN11744 , chapter 3 and chapter 5 for more details.
after you install the correct driver, you can update BootLoader_And_Nfcrdlib_SimplifiedAPI_EMVCo_Secondary.bin file, if you need to use cockpit.
Regards
Daniel
the VCOM driver is installed rightly!!! you can refer to above picture!