when I try to use " program lpc-link2 with segger j-link " to update the firmware, it will quit directly,so what should i do to make it show fig3
Hi,
Before you update the firmware, you should use jumper to connect jp5. When update successfully, remove it.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
hi
I did it, but it still doesn`t work. window of "Program LPC-Link2 with Segger J-Link" quit directly .Is it connected like this
Hi,
Do you connect the jumper without power?
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Yes, i connected jumper without power. Do I need an emulator?
Hi,
Update your lpcscrypt. lpc
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
thankyou a lot , i tried it again, but it showed me another problem. sorry ,could you tell me how to deal with it?
Hi,
This is the problem of the PATH environment variable. Adding the directory of the windows command to the PATH will overwrite. That is: append to the path: %SystemRoot%\system32;%SystemRoot%;
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
I have tried my best to do ,but it still someting wrong
hi ,it stope in here, and nothing happen.
Hi,
Do you press 'space' to start update?
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi,
Yes, i pressed the "space", it just moved to the next line.
Have a great day,
Hi,
Does your board work well? Can you download the program? If you do not connect the board, then press 'space', does it show something?
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
hi
yes,i can download program from IAR by CMSIS-DAP but cann`t use JLINK.
Hi,
Please go to '
Control Panel\Hardware and Sound\Devices and Printers'. Do you see something like this?
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------