qn9080sip use j-link

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

qn9080sip use j-link

1,841 次查看
1758793535
Contributor I

 when I try to use " program lpc-link2 with segger j-link " to update the firmware, it will quit directly,so what should i do to make it show  fig3   BKAH(I[]AP}AE5BWVDD8WUM.pngjlink.pngCX8JZTZ0RFCUQNQ)5CMNOKD.png

0 项奖励
回复
15 回复数

1,837 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

Before you update the firmware, you should use jumper to connect jp5. When update successfully, remove it.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

1,833 次查看
1758793535
Contributor I

hi

I did it, but it still doesn`t work. window of  "Program LPC-Link2 with Segger J-Link" quit directly .Is it connected like thislianjietu.jpg

0 项奖励
回复

1,825 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

Do you connect the jumper without power? 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

1,822 次查看
1758793535
Contributor I

Yes, i connected jumper without power. Do I need an emulator?

0 项奖励
回复

1,815 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

Update your lpcscrypt. lpc 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

1,810 次查看
1758793535
Contributor I

11.pngthankyou a lot  ,  i tried it again, but it showed me another problem. sorry ,could you tell me how to deal with it?

 

22.png

 

0 项奖励
回复

1,804 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

This is the problem of the PATH environment variable. Adding the directory of the windows command to the PATH will overwrite. That is: append to the path: %SystemRoot%\system32;%SystemRoot%;

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

1,799 次查看
1758793535
Contributor I

I have tried my best to do ,but it still someting wrongBL5%A(8Q$39RL$6{C3)YN83.png

0 项奖励
回复

1,789 次查看
nxf56274
NXP Employee
NXP Employee

3.PNG

0 项奖励
回复

1,782 次查看
1758793535
Contributor I

{A4ZQP]T)S5Q}%OFZ3P}6R6.pnghi ,it stope in here, and nothing happen.

0 项奖励
回复

1,756 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

Do you press  'space' to start update?

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

1,752 次查看
1758793535
Contributor I

Hi,

Yes,  i  pressed the "space", it just moved to the next line.

Have a great day,

0 项奖励
回复

1,747 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

Does your board work well? Can you download the program? If you do not connect the board, then press 'space', does it show something?

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

1,743 次查看
1758793535
Contributor I

hi

yes,i can download program from IAR by CMSIS-DAP  but cann`t use JLINK.

0 项奖励
回复

1,732 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

Please go to '

Control Panel\Hardware and Sound\Devices and Printers'. Do you see something like this? 

2.PNG

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复