Using Wi-fi STA and AP simultaneously.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using Wi-fi STA and AP simultaneously.

ソリューションへジャンプ
2,415件の閲覧回数
masakiyo
Contributor II

I am using JODY-W2 (88W8987).

I am using mlan0 and uap0 simultaneously.

The uap0 is used for streaming video.

When mlan0 performs SCAN, the throughput of uap0 decreases and streaming becomes disrupted.

I found out that the cause of this is that uap0's transmitter stops while mlan0 is doing SCAN. This was stated in the release notes (https://www.nxp.com.cn/docs/en/release-note/L6.1.36_2.1.0_WIFI-Doc.pdf).

 

Simultaneous Mode Operation Limitations

uAP/P2P-GO beacons are paused unconditionally whenever STA/P2P-GC performs scan and are resumed automatically once the scan is complete.

 

Block diagram of 88W8987 (https://www.nxp.jp/products/wireless-connectivity/wi-fi-plus-bluetooth-plus-802-15-4/2-4-5-ghz-dual-...), there was only one MAC. For this reason, I found out that it is not possible to send while receiving for SCAN.

 

What I would like you to tell me is the following.

Does AW-CM276NF (88W8997) have any of the above limitations? Looking at the block diagram(https://www.nxp.jp/products/wireless-connectivity/wi-fi-plus-bluetooth-plus-802-15-4/2-4-5-ghz-dual-...), it looks like there are two MACs.

 

Thank you.

0 件の賞賛
返信
1 解決策
2,402件の閲覧回数
ocourson
NXP TechSupport
NXP TechSupport

Dear @masakiyo 

 

All NXP Wifi/BT chipsets have only one Wifi MAC, expect 88W9098, which has 2 Wifi MACs.

 

Regards,

Olivier

元の投稿で解決策を見る

1 返信
2,403件の閲覧回数
ocourson
NXP TechSupport
NXP TechSupport

Dear @masakiyo 

 

All NXP Wifi/BT chipsets have only one Wifi MAC, expect 88W9098, which has 2 Wifi MACs.

 

Regards,

Olivier