UWB - MK UWB Mobile Edition Evaluation Kit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UWB - MK UWB Mobile Edition Evaluation Kit

1,370件の閲覧回数
patsn
Contributor I

With this module, I understand that I can use an iPhone and its U1 chip.

I have some questions :

- Is the kit is compatible with an Samsung S21 Ultra phone which has an embedded UWB chip ?

- Can I add a NFC shield to the arduino equiped with the UWB Tag SR040 ? The purpose is to exchange data between the arduino through NFC protocol when the arduino is close to an mobile phone. Is this possible to do so ? My project is to open through a small distance (50cm) calculated by UWB a door equiped with a NFC reader. I approach the door (50cm) my phone send data through Bluetooth for example, and the reader take the data sent and then open the door.

 

Is it a feasible project ?

タグ(4)
0 件の賞賛
返信
1 返信

1,342件の閲覧回数
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi,

 

Hope you are doing well. Could you please redirect your question to Mobile Knowledge?

They will be able to help you with the support of their kit.

 

Best Regards,

Ricardo

0 件の賞賛
返信