QN9080SIP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QN9080SIP

1,559 Views
1758793535
Contributor I

After successful connection, it will be disconnected automatically.pngAfter successful connection, it will be disconnected automatically。When connecting with another software that supports GATT protocol, it will be disconnected immediately after connecting

0 Kudos
Reply
1 Reply

1,545 Views
nxf56274
NXP Employee
NXP Employee

Hi,

You should install some apps. Use them to connect , or device will disconnect automatically.

I suggest you use this app 'nrf connect'.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply