I'm using MCUXpresso IDE v11.4.0.6224.
I installed SDK_2_6_3_JN5189DK6.
The tool works well in this point.
Next, I installed the Zigbee Configuration Editor plug-in.
And, I couldn't run the tool.
When I try to run the MCUXpresso IDE, the tool is automatically closed when it is opening.
I tried reinstall the tool after cleaning, 10 times, but it was the same every single time.
How do I use the MCUXpresso IDE with Zigbee Configuration Editor?
Solved! Go to Solution.
Self-Answered
It needs JRE.