Couldn't run MCUXpresso IDE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Couldn't run MCUXpresso IDE

Jump to solution
658 Views
sChameleoNz
Contributor III

I'm using MCUXpresso IDE v11.4.0.6224.

I installed SDK_2_6_3_JN5189DK6.

The tool works well in this point.

Next, I installed the Zigbee Configuration Editor plug-in.

And, I couldn't run the tool.

When I try to run the MCUXpresso IDE, the tool is automatically closed when it is opening.

I tried reinstall the tool after cleaning, 10 times, but it was the same every single time.

How do I use the MCUXpresso IDE with Zigbee Configuration Editor?

Labels (2)
0 Kudos
1 Solution
645 Views
sChameleoNz
Contributor III

Self-Answered

It needs JRE.

View solution in original post

1 Reply
646 Views
sChameleoNz
Contributor III

Self-Answered

It needs JRE.