Hi,
following AN14114, I am trying to run a a TX test with a carrier wave.
Firmware: SDIW612---18.99.2.p66.17-MM6X18437.p3-GPL-(FP92) on a 6.6 kernel.
I am sending the following lines one by one to /proc/mwlan/adapter0/config
rf_test_mode=1
radio_mode=11 0
rx_antenna=1
tx_antenna=1
band=0
bw=0
channel=4
tx_power=12 2 0
tx_continuous=1 1 0xaaa 0 3 0x2106
I see the waveform but when I try to stop the test with the following line, nothing happens, the DUT keeps transmitting.
tx_continuous=0
Note that in continuous packet mode (tx_continuous=1 0) I do not see this issue to stop the test.
This is quite inconvenient as I have to power cycle the chip every time I need to change the test channel.