Hi, @virti_choksi
Thanks for your trial.
I checked your new logs based on the method 1 to set psmode=0.
Yes, from the given logs, I saw you have set psmode=0 successfully, but still failed with same reason.
It looks like our FW doesn't response in time and result in tombstone.
Please see below my analysis.
===========
Successful scenario:
01-15 23:01:27.463 373 373 I hardware_nxp: Sending hci command 0x0C03 (hw_bt_send_reset)
01-15 23:01:27.871 373 11374 I hardware_nxp: Reply received for command 0x0C03 (hw_bt_send_reset) status 0x00
Failed scenario:
01-15 23:07:30.980 373 373 I hardware_nxp: Sending hci command 0x0C03 (hw_bt_send_reset)
01-15 23:07:33.856 11525 11550 E bt_hci : system/bt/hci/src/hci_layer.cc:379 startup_timer_expired: startup_timer_expired
==============
Please have a try with the second method, and let me know your result.
If still failed, please provide me same logs.
At the same time, I will also discuss this issue with our internal team to see what happened in the firmware side.
Best regards,
Christine.