BeeStack project size is too big (~100MB), I can't zip it to share it by email.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BeeStack project size is too big (~100MB), I can't zip it to share it by email.

1,605 Views
AlanCollins
Contributor V

Dear ZigBee developers, your problems are now solved :smileycool:

  • First you need to identify which library you are using:
    • Open your project (IAR or CodeWarrior),
    • Check on the ZigBee/Library folder, the library name is similar to “BeeStackZrRsRNPSp2_MC13226.a”,
  • Now you can delete other libraries inside the “....\ZigBee\Libs” (just don’t remove the one you are using).
  • Then you can use 7zip (freeware) to compress the files.


Instead of ~100MB, you will have a 7zip of ~2MB.


Enjoy :smileyhappy:

Labels (1)
Tags (1)
0 Kudos
Reply
0 Replies