Hi, @javadR3
Thanks for pointing us and drawing a very clear Pic to better understanding our Release.
P149.xxx is compiled on our R10.X branch.
P136.xxx is compiled on our R9.x branch.
It means, P149.xxx is newer than P136.xxx.
You can double confirm this point from our release note:
1. In the release note of:
PCIE-WLAN-UART-BT-9098-U16-X86-17.68.1.p136.58-17.26.1.p136.58-MXM5X17366_P32_V0V1-GPL
Bug Fixes/Feature Enhancements [Between R9.14 p136.57 to R9.15 p136.58]
2. In the release note of:
PCIE-WLAN-UART-BT-9098-U16-X86-17.68.1.p149.14-17.26.1.p149.14-MXM5X17405_P9_V0V1-GPL
Bug Fixes/Feature Enhancements [Between R10.2 p149.15 to R10.3 p149.20]
Conclusion:
So I suggest you to use this "PCIE-WLAN-UART-BT-9098-U16-X86-17.68.1.p149.20-17.26.1.p149.20-MXM5X17405_P16_V0V1-GPL" release for now, if you didn't have our P136.xxx release on your project and thinking about FP68 release, not FP92 release.
Hope it is clear for you, and have a nice day~
Best regards,
Christine.