Wireless Connectivity Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wireless Connectivity Knowledge Base

Discussions

Sort by:
       This document will address the JN5169 CMET setup and JN5169 connection setup with IQxel-MW. We also show the EVM and packet error rate results.
View full article
The border router device provides connectivity of the nodes in the Thread network with the possibility to connect to the networks as the www. Requirements Hardware K32W/JN5189 DK6 Board Udoo Neo Ethernet Cable Software MCUXpresso IDE v11.4.1 o newer. SDK 2.6.4. https://mcuxpresso.nxp.com/en/dashboard DK6 Production Flash Programmer Tool udoo_neo_os_nxp.img Docker Image Software Set up 1. Flash udoo_neo_os_nxp.img on an SD card using a tool. You could use any tool to flash the image, make sure that the SD card is correctly formatted. 2. Flash the ot-rcp.bin file on the USB Dongle(K32W/JN5189),  included in the SDK. \K32W061DK6\middleware\wireless\openthread\openthread\output\k32w061\bin DK6Programmer.exe -V5 -s COM2 -p ot-rcp.bin Running OpenThread BorderRouter You have connected your Udoo Neo board to an Ethernet cable, just open a new terminal to be sure that you have a connection. You could type the ping 8.8.8.8 command. If you do not have the IPV4, you could access connection your board to your computer and use the USB IP. After that, you could open a browser and enter to the Udoo Neo page using the USB IP. You could use the different address for creating a SSH connection.   Install Docker Copy the Docker image and Bash scripts to the Udoo Board; Install docker; curl -sSl https://get.docker.com | sh; The command will take some time   Verify the Docker images was successfully loaded Launch a Docker container   In this case, the UDOO NEO Extended doesn't have an Ethernet port, so, there is a USB converter to Ethernet. The OpenThread Example requires an IPV6 address sudo ./run_br_container.sh; Note: You have to have Ethernet Connection because the OpenThread requires IPV6. Be sure that the file has the execute permissions. The image below shows the process of the container. You cannot use this terminal, as this is a running Docker instance. It will output logs from the wpantund while it’s running.   Open a new terminal and look at for the container ID     After that, open a browser and search the IPV4 of your UDOO Neo, and you will find an OpenThread web page.     On the left side, select the option form, and a new page will be displayed for the network creation. Then you can ask for the wpanctl status, it will show all the Thread information, the address, the channel of the network, etc. sudo wpanctl status sudo wpanctl getprop Thread:OnMeshPrefixes Node A In the same UDOO terminal, start the border router internal commissioner and allow that a Thread node with the preshared key could join in this network. sudo wpanctl commissioner start; sudo wpanctl commissioner joiner-add “*” 120 J01NME; Node B Flash another JN5189/K32W using the REED example and type the next command for enabling and join to a Thread Network. \K32W061DK6\boards\k32w061dk6\wireless_examples\openthread\reed ifconfig up joiner start J01NME After the joining process is complete, type the next command to attach to the border router. thread start Look at the image below, you will notice the Node B Commands.   Ping the external internet 64:ff9b::808:808 to be sure that you have access to the internet.   For a better reference please look at the OpenThread Demo Applications User Guide included in your SDK documentation. "\K32W061DK6\docs\wireless\OpenThread" 11 Chapter Running Border Router Application Scenarios   Regards, Mario    
View full article
Please find here all the information needed to build your own PCB based on K32W061/041(AM/A), QN9090/9030(T) or JN5189/5188(T). Your first task before to send any inquiry to NXP support is to fill the K32W Design In CHECK LIST available in this ticket.   K32W061 Manufacturing package  Find here all the product pages, most of the HW documents are in the corresponding platforms web pages: K32W061/041 (AM/A) QN9090/9030(T) JN5189/5188(T)   The K32W EVK getting started webpage: IOT_ZTB-DK006 Get started page (nxp.com) IoT_ZTB getting started manual (nxp.com)   HW: HW design consideration : JN-RM-2078-JN5189-Module-Development_1V4.pdf (see attached file) JN-RM-2079-QN9090-Module-Development_1V0.pdf (see attached file) JN-RM-2080-K32W-Module-Development_1V0.pdf (see attached file)   Radio: RF report:  JN5189: https://www.nxp.com/docs/en/application-note/AN12154.pdf (nxp.com) QN9090: https://www.nxp.com/docs/en/nxp/application-notes/AN12610.pdf (nxp.com) K32W: https://www.nxp.com/docs/en/application-note/AN12798.pdf (nxp.com) Antenna: https://www.nxp.com/docs/en/application-note/AN2731.pdf (nxp.com)   Low Power Consumption:  JN5189: https://www.nxp.com/docs/en/application-note/AN12898.pdf (nxp.com) QN9090: https://www.nxp.com/docs/en/application-note/AN12902.pdf (nxp.com) K32W: https://www.nxp.com/docs/en/application-note/AN12846.pdf (nxp.com) A power calculator tool is available here: https://community.nxp.com/t5/Connectivity-Support-QN-JN-KW/QN9090-Bluetooth-LE-Power-Profile-Calculator-Tool/ta-p/1209602 SW tools: Customer Module Evaluation Tool  (nxp.com) Bluetooth Low Energy Certification Tool (nxp.com) K32W041/K32W061/QN9090(T)/QN9030(T) Bluetooth Low Energy Certification Tool User's Guide (nxp.com)     Certification: Certificates/Declarations of conformity (nxp community)  
View full article
This Application Note provides guidance on migrating ZigBee 3.0 Base device application designed for the NXP JN516x wireless microcontrollers to the KW41Z with the help of attached PDF.
View full article