requesting IW416 NXP Driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

requesting IW416 NXP Driver

29,813件の閲覧回数
naresh_nakka
Contributor I

Hi ,

i am working on wifi (iw416 chip -  LBEE5CJ1XK )

Interface : wifi - sdio , BT - uart .

could you please share the wifi-bt driver and firmware ?

also please mention what are changes required to enable it in the kernel ?

Thanks,

Naresh

 

0 件の賞賛
返信
39 返答(返信)

18,849件の閲覧回数
naresh_nakka
Contributor I

Hi NXP, 

Actually, i want to integrate this wifi driver in yocto build (has 6.1.80 linux kernel)

Could you please provide the meta-layer path for theese wifi driver ?

Thank, Naresh

 

0 件の賞賛
返信

18,826件の閲覧回数
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @naresh_nakka 

Can you please help to create a new thread to ask new questions?

This thread is last year, it is too old and can not automatically linked to our SFDC system for tracking further.

Thanks for your corporation and understandings.

 

Best regards,

Christine.

タグ(1)
0 件の賞賛
返信

18,816件の閲覧回数
naresh_nakka
Contributor I

Sure Christine Le.

 

BR, Naresh

0 件の賞賛
返信

20,426件の閲覧回数
naresh_nakka
Contributor I

HI @Christine_Li  ,

wifi firmware init is failing after reboot command in the kernel.

please help me on this.

please find the logs :

root@am62xx-evm:/home#
root@am62xx-evm:/home#
root@am62xx-evm:/home# insmod moal.ko fw_serial=1 fw_name=nxp/sdiouartiw416_combo_v0.bin cal_data_cfg=none ps_mode=1 auto_ds=1 host_mlme=1
[ 65.749348] wlan: Loading MWLAN driver
[ 65.753702] wlan: Register to Bus Driver...
[ 65.845021] vendor=0x02DF device=0x9159 class=0 function=1
[ 65.850973] Attach moal handle ops, card interface type: 0x108
[ 65.858121] rps set to 0 from module param
[ 65.862617] No module param cfg file specified
[ 65.867454] SDIO: max_segs=128 max_seg_size=65536
[ 65.872549] rx_work=1 cpu_num=4
[ 65.876186] Attach mlan adapter operations.card_type is 0x108.
[ 65.883522] wlan: Enable TX SG mode
[ 65.887497] wlan: Enable RX SG mode
[ 65.892863] Request firmware: nxp/sdiouartiw416_combo_v0.bin
[ 65.916775] WLAN FW already running! Skip FW download
[ 65.921927] WLAN FW is active
[ 65.925763] on_time is 65713086385
[ 71.092742] Timeout cmd id (70.880051) FUNC_INIT [0xa9], act = 0x0
[ 71.099056] a9
[ 71.099075] 00
[ 71.100927] 08
[ 71.102697] 00
[ 71.104462] 01
[ 71.106268] 00
[ 71.108036] 00
[ 71.109838] 00
[ 71.111606] 00
[ 71.113407] 00
[ 71.115174] 00
[ 71.116975] 00
[ 71.118742] 00
[ 71.120506] 00
[ 71.122306] 00
[ 71.124073] 00
[ 71.125873]
[ 71.129163] BSS type = 0 BSS role= 0
[ 71.132794] ------------Dump info-----------
[ 71.137109] Commmand Timeout
[ 71.140004] pending command id: 0x242 ioctl_buf=0000000000000000
[ 71.146031] pending command id: 0x3 ioctl_buf=0000000000000000
[ 71.151877] No pending scan command
[ 71.155409] mlan_processing =0
[ 71.158512] main_lock_flag =0
[ 71.161530] main_process_cnt =2
[ 71.164721] delay_task_flag =0
[ 71.167790] mlan_rx_processing =0
[ 71.171150] rx_pkts_queued=0
[ 71.174080] more_task_flag = 0
[ 71.177185] num_cmd_timeout = 1
[ 71.180341] last_cmd_index = 1
[ 71.183442] last_cmd_id =
[ 71.183455] 0x0
[ 71.186212] 0xa9
[ 71.188069] 0x0
[ 71.190043] 0x0
[ 71.191898] 0x0
[ 71.193784] 0x0
[ 71.195639] 0x0
[ 71.197525] 0x0
[ 71.199380] 0x0
[ 71.201266] 0x0
[ 71.203121]
[ 71.206497] last_cmd_act =
[ 71.206511] 0x0
[ 71.209352] 0x0
[ 71.211207] 0x0
[ 71.213094] 0x0
[ 71.214949] 0x0
[ 71.216837] 0x0
[ 71.218691] 0x0
[ 71.220543] 0x0
[ 71.222429] 0x0
[ 71.224283] 0x0
[ 71.226170]
[ 71.229547] last_cmd_resp_index = 0
[ 71.233083] last_cmd_resp_id =
[ 71.233097] 0x0
[ 71.236251] 0x0
[ 71.238137] 0x0
[ 71.239992] 0x0
[ 71.241877] 0x0
[ 71.243732] 0x0
[ 71.245619] 0x0
[ 71.247473] 0x0
[ 71.249359] 0x0
[ 71.251214] 0x0
[ 71.253099]
[ 71.256440] last_event_index = 0
[ 71.259713] last_event =
[ 71.259726] 0x0
[ 71.262394] 0x0
[ 71.264249] 0x0
[ 71.266136] 0x0
[ 71.267990] 0x0
[ 71.269876] 0x0
[ 71.271731] 0x0
[ 71.273617] 0x0
[ 71.275471] 0x0
[ 71.277359] 0x0
[ 71.279213]
[ 71.282588] num_data_h2c_failure = 0
[ 71.286210] num_cmd_h2c_failure = 0
[ 71.289749] num_data_c2h_failure = 0
[ 71.293372] num_cmdevt_c2h_failure = 0
[ 71.297170] num_int_read_failure = 0
[ 71.300792] last_int_status = 128
[ 71.304121] num_alloc_buffer_failure = 0
[ 71.308087] num_pkt_dropped = 0
[ 71.311277] num_no_cmd_node = 0
[ 71.314467] num_event_deauth = 0
[ 71.317742] num_event_disassoc = 0
[ 71.321191] num_event_link_lost = 0
[ 71.324726] num_cmd_deauth = 0
[ 71.327795] num_cmd_assoc_success = 0
[ 71.331502] num_cmd_assoc_failure = 0
[ 71.335211] num_cons_assoc_failure = 0
[ 71.339007] cmd_resp_received=0
[ 71.342197] event_received=0
[ 71.345128] max_tx_buf_size=2048
[ 71.348370] tx_buf_size=2048
[ 71.351295] curr_tx_buf_size=2048
[ 71.354658] data_sent=1 cmd_sent=0
[ 71.358113] ps_mode=1 ps_state=0
[ 71.361392] wakeup_dev_req=0 wakeup_tries=0 wakeup_timeout=0
[ 71.367103] hs_configured=0 hs_activated=0
[ 71.371247] pps_uapsd_mode=0 sleep_pd=0
[ 71.375134] tx_lock_flag = 0
[ 71.378064] scan_processing = 0
[ 71.381254] scan_state = 0x0
[ 71.384149] bypass_pkt_count=0
[ 71.387252] mp_rd_bitmap=0x0 curr_rd_port=0x0
[ 71.391659] mp_wr_bitmap=0x0 curr_wr_port=0x0
[ 71.396066] mp_data_port_mask = 0xffffffff
[ 71.400209] last_recv_rd_bitmap=0x0 mp_invalid_update=0
[ 71.405483] last_recv_wr_bitmap=0x0 last_mp_index=0
[ 71.410410] mp_wr_bitmap: 0x0 mp_wr_ports=0x0 len=0 curr_wr_port=0x0
[ 71.416820] 0x00
[ 71.416837] 0x00
[ 71.418778] 0x00
[ 71.420751] 0x00
[ 71.422693] 0x00
[ 71.424631] 0x00
[ 71.426603] 0x00
[ 71.428544] 0x00
[ 71.430517] 0x00
[ 71.432459] 0x00
[ 71.434433] 0x00
[ 71.436374] 0x00
[ 71.438347] 0x00
[ 71.440288] 0x00
[ 71.442261] 0x00
[ 71.444202] 0x00
[ 71.446175]
[ 71.449637] mp_wr_bitmap: 0x0 mp_wr_ports=0x0 len=0 curr_wr_port=0x0
[ 71.456046] 0x00
[ 71.456064] 0x00
[ 71.458038] 0x00
[ 71.459979] 0x00
[ 71.461952] 0x00
[ 71.463893] 0x00
[ 71.465867] 0x00
[ 71.467808] 0x00
[ 71.469782] 0x00
[ 71.471723] 0x00
[ 71.473696] 0x00
[ 71.475637] 0x00
[ 71.477610] 0x00
[ 71.479552] 0x00
[ 71.481525] 0x00
[ 71.483467] 0x00
[ 71.485441]
[ 71.488901] mp_wr_bitmap: 0x0 mp_wr_ports=0x0 len=0 curr_wr_port=0x0
[ 71.495310] 0x00
[ 71.495328] 0x00
[ 71.497302] 0x00
[ 71.499244] 0x00
[ 71.501217] 0x00
[ 71.503158] 0x00
[ 71.505132] 0x00
[ 71.507073] 0x00
[ 71.509047] 0x00
[ 71.510988] 0x00
[ 71.512960] 0x00
[ 71.514901] 0x00
[ 71.516875] 0x00
[ 71.518816] 0x00
[ 71.520791] 0x00
[ 71.522731] 0x00
[ 71.524670]
[ 71.528130] mp_wr_bitmap: 0x0 mp_wr_ports=0x0 len=0 curr_wr_port=0x0
[ 71.534537] 0x00
[ 71.534554] 0x00
[ 71.536494] 0x00
[ 71.538467] 0x00
[ 71.540409] 0x00
[ 71.542381] 0x00
[ 71.544322] 0x00
[ 71.546295] 0x00
[ 71.548236] 0x00
[ 71.550209] 0x00
[ 71.552150] 0x00
[ 71.554123] 0x00
[ 71.556065] 0x00
[ 71.558038] 0x00
[ 71.559980] 0x00
[ 71.561993] 0x00
[ 71.563937]
[ 71.567401] mp_wr_bitmap: 0x0 mp_wr_ports=0x0 len=0 curr_wr_port=0x0
[ 71.573808] 0x00
[ 71.573825] 0x00
[ 71.575765] 0x00
[ 71.577738] 0x00
[ 71.579680] 0x00
[ 71.581653] 0x00
[ 71.583594] 0x00
[ 71.585567] 0x00
[ 71.587509] 0x00
[ 71.589482] 0x00
[ 71.591424] 0x00
[ 71.593424] 0x00
[ 71.595367] 0x00
[ 71.597340] 0x00
[ 71.599281] 0x00
[ 71.601254] 0x00
[ 71.603195]
[ 71.606655] mp_wr_bitmap: 0x0 mp_wr_ports=0x0 len=0 curr_wr_port=0x0
[ 71.613061] 0x00
[ 71.613079] 0x00
[ 71.615019] 0x00
[ 71.616992] 0x00
[ 71.618933] 0x00
[ 71.620907] 0x00
[ 71.622848] 0x00
[ 71.624821] 0x00
[ 71.626762] 0x00
[ 71.628736] 0x00
[ 71.630678] 0x00
[ 71.632616] 0x00
[ 71.634588] 0x00
[ 71.636530] 0x00
[ 71.638503] 0x00
[ 71.640444] 0x00
[ 71.642418]
[ 71.645880] mp_wr_bitmap: 0x0 mp_wr_ports=0x0 len=0 curr_wr_port=0x0
[ 71.652290] 0x00
[ 71.652308] 0x00
[ 71.654282] 0x00
[ 71.656223] 0x00
[ 71.658196] 0x00
[ 71.660136] 0x00
[ 71.662111] 0x00
[ 71.664052] 0x00
[ 71.666026] 0x00
[ 71.667967] 0x00
[ 71.669940] 0x00
[ 71.671881] 0x00
[ 71.673855] 0x00
[ 71.675796] 0x00
[ 71.677769] 0x00
[ 71.679710] 0x00
[ 71.681683]
[ 71.685145] mp_wr_bitmap: 0x0 mp_wr_ports=0x0 len=0 curr_wr_port=0x0
[ 71.691554] 0x00
[ 71.691572] 0x00
[ 71.693545] 0x00
[ 71.695487] 0x00
[ 71.697460] 0x00
[ 71.699401] 0x00
[ 71.701373] 0x00
[ 71.703315] 0x00
[ 71.705288] 0x00
[ 71.707228] 0x00
[ 71.709201] 0x00
[ 71.711142] 0x00
[ 71.713116] 0x00
[ 71.715057] 0x00
[ 71.717031] 0x00
[ 71.718972] 0x00
[ 71.720945]
[ 71.724373] mp_wr_bitmap: 0x0 mp_wr_ports=0x0 len=0 curr_wr_port=0x0
[ 71.730781] 0x00
[ 71.730798] 0x00
[ 71.732774] 0x00
[ 71.734716] 0x00
[ 71.736654] 0x00
[ 71.738626] 0x00
[ 71.740567] 0x00
[ 71.742540] 0x00
[ 71.744482] 0x00
[ 71.746454] 0x00
[ 71.748396] 0x00
[ 71.750369] 0x00
[ 71.752310] 0x00
[ 71.754283] 0x00
[ 71.756224] 0x00
[ 71.758197] 0x00
[ 71.760138]
[ 71.763598] mp_wr_bitmap: 0x0 mp_wr_ports=0x0 len=0 curr_wr_port=0x0
[ 71.770007] 0x00
[ 71.770024] 0x00
[ 71.771963] 0x00
[ 71.773936] 0x00
[ 71.775877] 0x00
[ 71.777850] 0x00
[ 71.779791] 0x00
[ 71.781763] 0x00
[ 71.783705] 0x00
[ 71.785679] 0x00
[ 71.787620] 0x00
[ 71.789593] 0x00
[ 71.791534] 0x00
[ 71.793506] 0x00
[ 71.795448] 0x00
[ 71.797420] 0x00
[ 71.799362]
[ 71.802824] bss_index = 0, tx_pkts_queued = 0
[ 71.807232] -------- Dump info End---------
[ 71.813517] SDIO Func0 (0x0-0x9): 43 03 02 02 03 00 08 02 03 00
[ 71.829061] SDIO Func1 (0x10-0x17): 00 00 00 00 ff ff ff ff
[ 71.841240] SDIO Func1: (0x8) c3 (0x58) 00 (0x5c) 48 (0x5d) 00 (0x60) 07 (0x61) 0c (0x62) 00 (0x64) 10 (0x65) 00 (0x66) 00 (0x68) 00 (0x69) 00 (0x6a) 00
[ 71.869159] SDIO Func1 (0xe8-0xf2): dc fe db 00 8b 00 3f 01 01 01 70
[ 71.989738] SDIO Func1 (0xe8-0xf2): dc fe e7 00 97 00 3f 01 01 01 70
[ 71.996313] woal_request_fw failed
[ 72.000109] Firmware Init Failed
[ 72.004202] Free module params
[ 72.007594] woal_add_card failed
[ 72.011081] wlan_sdio: probe of mmc2:0001:1 failed with error -1
[ 72.023589] wlan: Register to Bus Driver Done
[ 72.031002] wlan: Driver loaded successfully
root@am62xx-evm:/home#
CTRL-A Z for help | 115200 8N1 | NOR | Minicom 2.7.1 | VT102 | Offline | ttyUSB0

Thanks,

Naresh

0 件の賞賛
返信

20,413件の閲覧回数
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @naresh_nakka 

Can you please help to create a new case to us to ask the new issue?

And also please help to provide fw_dump at the same time for tracking this issue's root cause.

 

Best regards,

Christine.

タグ(1)
0 件の賞賛
返信

20,896件の閲覧回数
naresh_nakka
Contributor I

Hi , 

some times i am gettings below issue.  please help me on this.

root@am62xx-evm:/home# insmod moal.ko mod_para=nxp/wifi_mod_para.conf
[ 1051.997768] wlan: Loading MWLAN driver
[ 1052.002112] wlan: Register to Bus Driver...
[ 1052.089234] vendor=0x02DF device=0x9159 class=0 function=1
[ 1052.094989] Attach moal handle ops, card interface type: 0x108
[ 1052.101639] rps set to 0 from module param
[ 1052.106444] SDIW416: init module param from usr cfg
[ 1052.112021] card_type: SDIW416, config block: 0
[ 1052.116961] cfg80211_wext=0xf
[ 1052.120485] max_vir_bss=1
[ 1052.123439] cal_data_cfg=none
[ 1052.126657] ps_mode = 1
[ 1052.129104] auto_ds = 1
[ 1052.131958] host_mlme=enable
[ 1052.135089] fw_name=nxp/sdiouartiw416_combo_v0.bin
[ 1052.140166] SDIO: max_segs=128 max_seg_size=65536
[ 1052.145225] rx_work=1 cpu_num=4
[ 1052.148647] Attach mlan adapter operations.card_type is 0x108.
[ 1052.155297] wlan: Enable TX SG mode
[ 1052.159040] wlan: Enable RX SG mode
[ 1052.166285] Request firmware: nxp/sdiouartiw416_combo_v0.bin
[ 1052.430414] Wlan: FW download over, firmwarelen=534196 downloaded 534196
[ 1053.711382] Fail to poll firmware status: firmwarestat=0x5f5f
[ 1053.717161] FW failed to be active in time!
[ 1053.721969] wlan_dnld_fw fail ret=0xffffffff
[ 1053.726429] WLAN: Fail download FW with nowwait: 0
[ 1053.731584] SDIO Func0 (0x0-0x9): ERR
[ 1053.735518] SDIO Func1 (0x10-0x17): ERR
[ 1053.739597] SDIO Func1: (0x8) ERR
[ 1053.743147] SDIO Func1 (0xe8-0xf2): ERR
[ 1053.847253] SDIO Func1 (0xe8-0xf2): ERR
[ 1053.851212] woal_request_fw failed
[ 1053.854870] Firmware Init Failed
[ 1053.859000] Free module params
[ 1053.862066] woal_add_card failed
[ 1053.865890] wlan_sdio: probe of mmc2:0001:1 failed with error -1
[ 1053.875115] wlan: Register to Bus Driver Done
[ 1053.881259] wlan: Driver loaded successfully

Thanks,

Naresh

 

0 件の賞賛
返信

20,877件の閲覧回数
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @naresh_nakka 

From the given logs, we see that:

[ 1053.862066] woal_add_card failed
[ 1053.865890] wlan_sdio: probe of mmc2:0001:1 failed with error -1

It seems that the Wi-Fi card is not detected, please check your SDIO side connection, make sure the VIO_SD voltage is correct and connection is no problem. We need full dmesg logs for further check.

 

Best regards,

Christine.

タグ(1)
0 件の賞賛
返信

20,869件の閲覧回数
naresh_nakka
Contributor I

Hi ,

please find complete logs ,

root@am62xx-evm:~# dmesg
[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[ 0.000000] Linux version 6.1.33-00001-ge4769b223d98-dirty (naresh@naresh-ThinkPad-E15-Gen-2) (aarch64-none-linux-gnu-gcc (Arm GNU Toolchain 11.3.Rel1) 11.3.1 20220712, GNU ld (Arm GNU Toolchain 11.33
[ 0.000000] Machine model: Texas Instruments AM625 SK i2c can LTE TESSOLVE
[ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
[ 0.000000] printk: bootconsole [ns16550a0] enabled
[ 0.000000] efi: UEFI not found.
[ 0.000000] Reserved memory: created CMA memory pool at 0x00000000f7600000, size 128 MiB
[ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x000000009c800000, size 3 MiB
[ 0.000000] OF: reserved mem: initialized node ipc-memories@9c800000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x000000009cb00000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node m4f-dma-memory@9cb00000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x000000009cc00000, size 14 MiB
[ 0.000000] OF: reserved mem: initialized node m4f-memory@9cc00000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x000000009da00000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@9da00000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x000000009db00000, size 12 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@9db00000, compatible id shared-dma-pool
[ 0.000000] NUMA: No NUMA configuration found
[ 0.000000] NUMA: Faking a node at [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] NUMA: NODE_DATA [mem 0xf730fa00-0xf7311fff]
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] DMA32 empty
[ 0.000000] Normal empty
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080000000-0x000000009c7fffff]
[ 0.000000] node 0: [mem 0x000000009c800000-0x000000009e6fffff]
[ 0.000000] node 0: [mem 0x000000009e700000-0x000000009e77ffff]
[ 0.000000] node 0: [mem 0x000000009e780000-0x000000009fffffff]
[ 0.000000] node 0: [mem 0x00000000a0000000-0x00000000ff6fffff]
[ 0.000000] node 0: [mem 0x00000000ff700000-0x00000000fffc9fff]
[ 0.000000] node 0: [mem 0x00000000fffca000-0x00000000ffffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: Trusted OS migration not required
[ 0.000000] psci: SMC Calling Convention v1.2
[ 0.000000] percpu: Embedded 20 pages/cpu s44968 r8192 d28760 u81920
[ 0.000000] pcpu-alloc: s44968 r8192 d28760 u81920 alloc=20*4096
[ 0.000000] pcpu-alloc: [0] 0 [0] 1 [0] 2 [0] 3
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] CPU features: detected: ARM erratum 845719
[ 0.000000] alternatives: applying boot alternatives
[ 0.000000] Fallback order for Node 0: 0
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 516096
[ 0.000000] Policy zone: DMA
[ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=spi-nand0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),256k(ospi.env),256k(ospi.env.backup),9t
[ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] Memory: 1821060K/2097152K available (16512K kernel code, 3774K rwdata, 9032K rodata, 7616K init, 617K bss, 145020K reserved, 131072K cma-reserved)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4.
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] Tracing variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 256 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] Root IRQ handler: gic_handle_irq
[ 0.000000] GICv3: GICv3 features: 16 PPIs
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001880000
[ 0.000000] ITS [mem 0x01820000-0x0182ffff]
[ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[ 0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
[ 0.000000] ITS@0x0000000001820000: allocated 524288 Devices @80800000 (flat, esz 8, psz 64K, shr 0)
[ 0.000000] ITS: using cache flushing for cmd queue
[ 0.000000] GICv3: using LPI property table @0x0000000080040000
[ 0.000000] GIC: using cache flushing for LPI property table
[ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000080050000
[ 0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
[ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
[ 0.000000] sched_clock: 58 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
[ 0.009658] Console: colour dummy device 80x25
[ 0.014295] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
[ 0.024980] pid_max: default: 32768 minimum: 301
[ 0.029762] LSM: Security Framework initializing
[ 0.034604] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.042188] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.052044] cblist_init_generic: Setting adjustable number of callback queues.
[ 0.059500] cblist_init_generic: Setting shift to 2 and lim to 1.
[ 0.065798] cblist_init_generic: Setting shift to 2 and lim to 1.
[ 0.072217] rcu: Hierarchical SRCU implementation.
[ 0.077124] rcu: Max phase no-delay instances is 1000.
[ 0.082717] Platform MSI: msi-controller@1820000 domain created
[ 0.089043] PCI/MSI: /bus@f0000/interrupt-controller@1800000/msi-controller@1820000 domain created
[ 0.098319] fsl-mc MSI: msi-controller@1820000 domain created
[ 0.106197] EFI services will not be available.
[ 0.111155] smp: Bringing up secondary CPUs ...
[ 5.139080] CPU1: failed to come online
[ 5.143006] CPU1: failed in unknown state : 0x0
[ 10.266984] CPU2: failed to come online
[ 10.270909] CPU2: failed in unknown state : 0x0
[ 15.394886] CPU3: failed to come online
[ 15.398807] CPU3: failed in unknown state : 0x0
[ 15.403506] smp: Brought up 1 node, 1 CPU
[ 15.407619] SMP: Total of 1 processors activated.
[ 15.412443] CPU features: detected: 32-bit EL0 Support
[ 15.417698] CPU features: detected: 32-bit EL1 Support
[ 15.422957] CPU features: detected: CRC32 instructions
[ 15.428284] CPU: All CPU(s) started at EL2
[ 15.432489] alternatives: applying system-wide alternatives
[ 15.440386] devtmpfs: initialized
[ 15.452177] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 15.462201] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[ 15.473761] pinctrl core: initialized pinctrl subsystem
[ 15.481409] DMI not present or invalid.
[ 15.486079] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[ 15.493090] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations
[ 15.500464] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 15.508532] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 15.516708] audit: initializing netlink subsys (disabled)
[ 15.523875] thermal_sys: Registered thermal governor 'step_wise'
[ 15.523888] thermal_sys: Registered thermal governor 'power_allocator'
[ 15.530086] audit: type=2000 audit(15.412:1): state=initialized audit_enabled=0 res=1
[ 15.544851] cpuidle: using governor menu
[ 15.549114] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 15.556105] ASID allocator initialised with 65536 entries
[ 15.563415] Serial: AMBA PL011 UART driver
[ 15.587262] platform 30200000.dss: Fixed dependency cycle(s) with /bus@f0000/i2c@20010000/sii9022@3b
[ 15.600918] platform connector: Fixed dependency cycle(s) with /bus@f0000/i2c@20010000/sii9022@3b
[ 15.611386] KASLR disabled due to lack of seed
[ 15.624280] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
[ 15.631344] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
[ 15.637759] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
[ 15.644699] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
[ 15.651107] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
[ 15.658045] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
[ 15.664453] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
[ 15.671393] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
[ 15.679746] ACPI: Interpreter disabled.
[ 15.685756] k3-chipinfo 43000014.chipid: Family:AM62X rev:SR1.0 JTAGID[0x0bb7e02f] Detected
[ 15.696009] iommu: Default domain type: Translated
[ 15.701049] iommu: DMA domain TLB invalidation policy: strict mode
[ 15.707755] SCSI subsystem initialized
[ 15.711737] libata version 3.00 loaded.
[ 15.711967] usbcore: registered new interface driver usbfs
[ 15.717627] usbcore: registered new interface driver hub
[ 15.723083] usbcore: registered new device driver usb
[ 15.729564] pps_core: LinuxPPS API ver. 1 registered
[ 15.734652] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>
[ 15.744003] PTP clock support registered
[ 15.748141] EDAC MC: Ver: 3.0.0
[ 15.753190] omap-mailbox 29000000.mailbox: omap mailbox rev 0x66fc9100
[ 15.760700] FPGA manager framework
[ 15.764306] Advanced Linux Sound Architecture Driver Initialized.
[ 15.771584] vgaarb: loaded
[ 15.774858] clocksource: Switched to clocksource arch_sys_counter
[ 15.781380] VFS: Disk quotas dquot_6.6.0
[ 15.785434] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 15.792649] pnp: PnP ACPI: disabled
[ 15.801366] NET: Registered PF_INET protocol family
[ 15.806668] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear)
[ 15.816015] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear)
[ 15.824833] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
[ 15.832770] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear)
[ 15.840971] TCP bind hash table entries: 16384 (order: 7, 524288 bytes, linear)
[ 15.848965] TCP: Hash tables configured (established 16384 bind 16384)
[ 15.855891] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)
[ 15.862807] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)
[ 15.870329] NET: Registered PF_UNIX/PF_LOCAL protocol family
[ 15.876628] RPC: Registered named UNIX socket transport module.
[ 15.882736] RPC: Registered udp transport module.
[ 15.887547] RPC: Registered tcp transport module.
[ 15.892355] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 15.898946] NET: Registered PF_XDP protocol family
[ 15.903878] PCI: CLS 0 bytes, default 64
[ 15.908930] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available
[ 15.918092] kvm [1]: IPA Size Limit: 40 bits
[ 15.924009] kvm [1]: vgic-v2@100010000
[ 15.927887] kvm [1]: GIC system register CPU interface enabled
[ 15.933893] kvm [1]: vgic interrupt IRQ9
[ 15.937931] kvm [1]: Hyp mode initialized successfully
[ 15.944634] Initialise system trusted keyrings
[ 15.949488] workingset: timestamp_bits=42 max_order=19 bucket_order=0
[ 15.961930] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 15.968584] NFS: Registering the id_resolver key type
[ 15.973818] Key type id_resolver registered
[ 15.978097] Key type id_legacy registered
[ 15.982262] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 15.989119] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[ 15.996896] 9p: Installing v9fs 9p2000 file system support
[ 16.035662] Key type asymmetric registered
[ 16.039852] Asymmetric key parser 'x509' registered
[ 16.044891] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244)
[ 16.052635] io scheduler mq-deadline registered
[ 16.057281] io scheduler kyber registered
[ 16.070816] pinctrl-single 4084000.pinctrl: 34 pins, size 136
[ 16.077474] pinctrl-single f4000.pinctrl: 171 pins, size 684
[ 16.084346] pinctrl-single a40000.pinctrl: 512 pins, size 2048
[ 16.099063] EINJ: ACPI disabled.
[ 16.128557] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 16.138963] SuperH (H)SCI(F) driver initialized
[ 16.144364] msm_serial: driver initialized
[ 16.156155] loop: module loaded
[ 16.161310] megasas: 07.719.03.00-rc1
[ 16.173216] tun: Universal TUN/TAP device driver, 1.6
[ 16.178721] CAN device driver interface
[ 16.183871] thunder_xcv, ver 1.0
[ 16.187242] thunder_bgx, ver 1.0
[ 16.190568] nicpf, ver 1.0
[ 16.194944] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version
[ 16.202397] hns3: Copyright (c) 2017 Huawei Corporation.
[ 16.207903] hclge is initializing
[ 16.211316] e1000: Intel(R) PRO/1000 Network Driver
[ 16.216303] e1000: Copyright (c) 1999-2006 Intel Corporation.
[ 16.222207] e1000e: Intel(R) PRO/1000 Network Driver
[ 16.227282] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 16.233375] igb: Intel(R) Gigabit Ethernet Network Driver
[ 16.238895] igb: Copyright (c) 2007-2014 Intel Corporation.
[ 16.244620] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[ 16.251029] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 16.257557] sky2: driver version 1.30
[ 16.262975] VFIO - User Level meta-driver version: 0.3
[ 16.271149] usbcore: registered new interface driver usb-storage
[ 16.280891] i2c_dev: i2c /dev entries driver
[ 16.296306] sdhci: Secure Digital Host Controller Interface driver
[ 16.302695] sdhci: Copyright(c) Pierre Ossman
[ 16.308359] Synopsys Designware Multimedia Card Interface Driver
[ 16.315821] sdhci-pltfm: SDHCI platform and OF driver helper
[ 16.324284] ledtrig-cpu: registered to indicate activity on CPUs
[ 16.332595] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[ 16.340133] usbcore: registered new interface driver usbhid
[ 16.345863] usbhid: USB HID core driver
[ 16.356165] optee: probing for conduit method.
[ 16.360846] optee: revision 3.20 (8e74d476)
[ 16.361170] optee: dynamic shared memory is enabled
[ 16.370698] optee: initialized driver
[ 16.375150] gnss: GNSS driver registered with major 509
[ 16.380598] usbcore: registered new interface driver gnss-usb
[ 16.390254] Initializing XFRM netlink socket
[ 16.394793] NET: Registered PF_PACKET protocol family
[ 16.399985] can: controller area network core
[ 16.404534] NET: Registered PF_CAN protocol family
[ 16.409590] 9pnet: Installing 9P2000 support
[ 16.414031] Key type dns_resolver registered
[ 16.418916] registered taskstats version 1
[ 16.423138] Loading compiled-in X.509 certificates
[ 16.478578] ti-sci 44043000.system-controller: ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)')
[ 16.567939] omap_i2c 4900000.i2c: bus 0 rev0.12 at 400 kHz
[ 16.575267] omap_i2c 2b200000.i2c: bus 1 rev0.12 at 400 kHz
[ 16.607139] rtc-abx80x 2-0069: model 1805, revision 2.3, lot 347, wafer 13, uid 67f5
[ 16.615313] rtc-abx80x 2-0069: Enabling trickle charger: 05
[ 16.621814] rtc-abx80x 2-0069: Oscillator failure, data is invalid.
[ 16.628327] rtc-abx80x 2-0069: registered as rtc0
[ 16.633407] rtc-abx80x 2-0069: Oscillator failure, data is invalid.
[ 16.639817] rtc-abx80x 2-0069: hctosys: unable to read the hardware clock
[ 16.646822] omap_i2c 20000000.i2c: bus 2 rev0.12 at 400 kHz
[ 16.679371] omap_i2c 20010000.i2c: bus 3 rev0.12 at 100 kHz
[ 16.686996] omap_i2c 20020000.i2c: bus 4 rev0.12 at 400 kHz
[ 16.693526] ti-sci-intr 4210000.interrupt-controller: Interrupt Router 5 domain created
[ 16.702254] ti-sci-intr bus@f0000:interrupt-controller@a00000: Interrupt Router 3 domain created
[ 16.711865] ti-sci-inta 48000000.interrupt-controller: Interrupt Aggregator domain 28 created
[ 16.724589] ti-udma 485c0100.dma-controller: Number of rings: 82
[ 16.732822] ti-udma 485c0100.dma-controller: Channels: 48 (bchan: 18, tchan: 12, rchan: 18)
[ 16.745133] ti-udma 485c0000.dma-controller: Number of rings: 150
[ 16.755248] ti-udma 485c0000.dma-controller: Channels: 35 (tchan: 20, rchan: 15)
[ 16.768401] printk: console [ttyS2] disabled
[ 16.772914] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 241, base_baud = 3000000) is a 8250
[ 16.781832] printk: console [ttyS2] enabled
[ 16.790293] printk: bootconsole [ns16550a0] disabled
[ 16.803188] 2810000.serial: ttyS3 at MMIO 0x2810000 (irq = 243, base_baud = 3000000) is a 8250
[ 16.817112] spi-nor spi0.0: unrecognized JEDEC id bytes: ff ff ff ff ff ff
[ 16.827080] m_can_platform 20701000.can: m_can device registered (irq=246, version=32)
[ 16.840017] davinci_mdio 8000f00.mdio: Configuring MDIO in manual mode
[ 16.886896] davinci_mdio 8000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[ 16.896293] davinci_mdio 8000f00.mdio: phy[0]: device 8000f00.mdio:00, driver unknown
[ 16.904211] davinci_mdio 8000f00.mdio: phy[1]: device 8000f00.mdio:01, driver unknown
[ 16.912121] am65-cpsw-nuss 8000000.ethernet: initializing am65 cpsw nuss version 0x6BA01103, cpsw version 0x6BA81103 Ports: 3 quirks:00000006
[ 16.925148] am65-cpsw-nuss 8000000.ethernet: Use random MAC address
[ 16.931437] am65-cpsw-nuss 8000000.ethernet: initialized cpsw ale version 1.5
[ 16.938565] am65-cpsw-nuss 8000000.ethernet: ALE Table size 512
[ 16.945071] pps pps0: new PPS source ptp0
[ 16.949340] am65-cpsw-nuss 8000000.ethernet: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:1
[ 16.959735] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 19
[ 16.977959] cpufreq: cpufreq_online: CPU0: Running at unlisted initial frequency: 1250000 KHz, changing to: 1000000 KHz
[ 17.001363] mmc0: CQHCI version 5.10
[ 17.005713] mmc1: CQHCI version 5.10
[ 17.020741] mmc2: CQHCI version 5.10
[ 17.033190] st_lsm6dsx_i2c 0-006b: supply vdd not found, using dummy regulator
[ 17.040699] st_lsm6dsx_i2c 0-006b: supply vddio not found, using dummy regulator
[ 17.058203] mmc0: SDHCI controller on fa10000.mmc [fa10000.mmc] using ADMA 64-bit
[ 17.078244] mmc2: SDHCI controller on fa20000.mmc [fa20000.mmc] using ADMA 64-bit
[ 17.129409] mmc2: new ultra high speed DDR50 SDIO card at address 0001
[ 17.138518] mmc0: new HS200 MMC card at address 0001
[ 17.144345] mmcblk0: mmc0:0001 MMC04G 3.58 GiB
[ 17.152831] mmcblk0: p1
[ 17.156244] mmcblk0boot0: mmc0:0001 MMC04G 16.0 MiB
[ 17.163040] mmcblk0boot1: mmc0:0001 MMC04G 16.0 MiB
[ 17.169344] mmcblk0rpmb: mmc0:0001 MMC04G 128 KiB, chardev (510:0)
[ 17.606591] pca953x 3-0022: supply vcc not found, using dummy regulator
[ 17.613507] pca953x 3-0022: using AI
[ 17.617367] pca953x 3-0022: failed writing register
[ 17.622516] pca953x: probe of 3-0022 failed with error -121
[ 17.632420] 4a00000.serial: ttyS0 at MMIO 0x4a00000 (irq = 433, base_baud = 3000000) is a 8250
[ 17.644993] omap8250 2820000.serial: PM domain pd:153 will not be powered off
[ 17.652723] 2820000.serial: ttyS1 at MMIO 0x2820000 (irq = 434, base_baud = 3000000) is a 8250
[ 17.666180] debugfs: Directory 'pd:182' with parent 'pm_genpd' already present!
[ 17.689773] ALSA device list:
[ 17.692817] No soundcards found.
[ 18.536096] sdhci-am654 fa00000.mmc: Power on failed
[ 18.572202] mmc1: SDHCI controller on fa00000.mmc [fa00000.mmc] using ADMA 64-bit
[ 19.111123] EXT4-fs (mmcblk0p1): recovery complete
[ 19.118030] EXT4-fs (mmcblk0p1): mounted filesystem with ordered data mode. Quota mode: none.
[ 19.126636] VFS: Mounted root (ext4 filesystem) on device 179:1.
[ 19.137921] devtmpfs: mounted
[ 19.146422] Freeing unused kernel memory: 7616K
[ 19.151192] Run /sbin/init as init process
[ 19.155304] with arguments:
[ 19.155308] /sbin/init
[ 19.155312] with environment:
[ 19.155315] HOME=/
[ 19.155319] TERM=linux
[ 19.367913] systemd[1]: System time before build time, advancing clock.
[ 19.423495] systemd[1]: systemd 250.5+ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -)
[ 19.455907] systemd[1]: Detected architecture arm64.
[ 19.516622] systemd[1]: Hostname set to <am62xx-evm>.
[ 19.761976] systemd-sysv-generator[151]: SysV service '/etc/init.d/netperf' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include .
[ 19.799925] systemd-sysv-generator[151]: SysV service '/etc/init.d/thermal-zone-init' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package t.
[ 19.835574] systemd-sysv-generator[151]: SysV service '/etc/init.d/psplash.sh' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to inclu.
[ 19.860029] systemd-sysv-generator[151]: SysV service '/etc/init.d/docker.init' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to incl.
[ 19.884400] systemd-sysv-generator[151]: SysV service '/etc/init.d/resize_rootfs.sh' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to.
[ 19.909059] systemd-sysv-generator[151]: SysV service '/etc/init.d/dropbear' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include.
[ 19.936018] systemd-sysv-generator[151]: SysV service '/etc/init.d/inetd.busybox' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to in.
[ 19.960501] systemd-sysv-generator[151]: SysV service '/etc/init.d/telnetd' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include .
[ 20.299792] systemd[1]: Binding to IPv6 address not available since kernel does not support IPv6.
[ 20.308783] systemd[1]: Binding to IPv6 address not available since kernel does not support IPv6.
[ 20.396822] systemd[1]: /etc/systemd/system/sync-clocks.service:11: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the.
[ 20.453718] systemd[1]: Binding to IPv6 address not available since kernel does not support IPv6.
[ 20.498072] systemd[1]: Queued start job for default target Multi-User System.
[ 20.584523] systemd[1]: Created slice Slice /system/getty.
[ 20.610571] systemd[1]: Created slice Slice /system/modprobe.
[ 20.634748] systemd[1]: Created slice Slice /system/serial-getty.
[ 20.658037] systemd[1]: Created slice User and Session Slice.
[ 20.679546] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ 20.703613] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ 20.727653] systemd[1]: Reached target Path Units.
[ 20.747144] systemd[1]: Reached target Remote File Systems.
[ 20.767399] systemd[1]: Reached target Slice Units.
[ 20.787272] systemd[1]: Reached target Swaps.
[ 20.841694] systemd[1]: Listening on RPCbind Server Activation Socket.
[ 20.863306] systemd[1]: Reached target RPC Port Mapper.
[ 20.900958] systemd[1]: Listening on Process Core Dump Socket.
[ 20.924108] systemd[1]: Listening on initctl Compatibility Named Pipe.
[ 20.949061] systemd[1]: Listening on Journal Audit Socket.
[ 20.972475] systemd[1]: Listening on Journal Socket (/dev/log).
[ 20.996490] systemd[1]: Listening on Journal Socket.
[ 21.021045] systemd[1]: Listening on Network Service Netlink Socket.
[ 21.045322] systemd[1]: Listening on udev Control Socket.
[ 21.068748] systemd[1]: Listening on udev Kernel Socket.
[ 21.093690] systemd[1]: Listening on User Database Manager Socket.
[ 21.143557] systemd[1]: Mounting Huge Pages File System...
[ 21.183598] systemd[1]: Mounting POSIX Message Queue File System...
[ 21.227638] systemd[1]: Mounting Kernel Debug File System...
[ 21.256381] systemd[1]: Kernel Trace File System was skipped because of a failed condition check (ConditionPathExists=/sys/kernel/tracing).
[ 21.287598] systemd[1]: Mounting Temporary Directory /tmp...
[ 21.316160] systemd[1]: Create List of Static Device Nodes was skipped because of a failed condition check (ConditionFileNotEmpty=/lib/modules/6.1.33-00001-ge4769b223d98-dirty/modules.devname).
[ 21.355857] systemd[1]: Starting Load Kernel Module configfs...
[ 21.403748] systemd[1]: Starting Load Kernel Module drm...
[ 21.447775] systemd[1]: Starting Load Kernel Module fuse...
[ 21.504545] systemd[1]: Starting Start psplash boot splash screen...
[ 21.549384] systemd[1]: Starting RPC Bind...
[ 21.571450] systemd[1]: File System Check on Root Device was skipped because of a failed condition check (ConditionPathIsReadWrite=!/).
[ 21.604837] systemd[1]: Starting Journal Service...
[ 21.664122] systemd[1]: Starting Load Kernel Modules...
[ 21.703963] systemd[1]: Starting Generate network units from Kernel command line...
[ 21.752229] systemd[1]: Starting Remount Root and Kernel File Systems...
[ 21.800377] systemd[1]: Starting Coldplug All udev Devices...
[ 21.850581] systemd[1]: Started RPC Bind.
[ 21.875957] systemd[1]: Mounted Huge Pages File System.
[ 21.903963] systemd[1]: Mounted POSIX Message Queue File System.
[ 21.931979] systemd[1]: Mounted Kernel Debug File System.
[ 21.962454] systemd[1]: Mounted Temporary Directory /tmp.
[ 21.979617] EXT4-fs (mmcblk0p1): re-mounted. Quota mode: none.
[ 22.004729] systemd[1]: [email protected]: Deactivated successfully.
[ 22.023249] systemd[1]: Finished Load Kernel Module configfs.
[ 22.059438] systemd[1]: [email protected]: Deactivated successfully.
[ 22.075515] systemd[1]: Finished Load Kernel Module drm.
[ 22.104758] systemd[1]: [email protected]: Deactivated successfully.
[ 22.120459] systemd[1]: Finished Load Kernel Module fuse.
[ 22.151995] systemd[1]: psplash-start.service: Main process exited, code=exited, status=255/EXCEPTION
[ 22.172046] systemd[1]: psplash-start.service: Failed with result 'exit-code'.
[ 22.191306] systemd[1]: Failed to start Start psplash boot splash screen.
[ 22.239166] systemd[1]: Dependency failed for Start psplash-systemd progress communication helper.
[ 22.271153] systemd[1]: psplash-systemd.service: Job psplash-systemd.service/start failed with result 'dependency'.
[ 22.292148] systemd[1]: Started Journal Service.
[ 22.565119] systemd-journald[164]: Received client request to flush runtime journal.
[ 22.777610] audit: type=1334 audit(1651167748.408:2): prog-id=5 op=LOAD
[ 22.794138] audit: type=1334 audit(1651167748.416:3): prog-id=6 op=LOAD
[ 23.942956] random: crng init done
[ 25.256725] audit: type=1334 audit(1651173074.944:4): prog-id=7 op=LOAD
[ 25.272363] audit: type=1334 audit(1651173074.952:5): prog-id=8 op=LOAD
[ 32.575647] am65-cpsw-nuss 8000000.ethernet eth1: PHY [8000f00.mdio:01] driver [Generic PHY] (irq=POLL)
[ 32.594805] am65-cpsw-nuss 8000000.ethernet eth1: configuring for phy/rgmii-rxid link mode
[ 32.626249] am65-cpsw-nuss 8000000.ethernet eth1: Link is Up - 100Mbps/Full - flow control rx/tx
[ 32.718309] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:00] driver [Generic PHY] (irq=POLL)
[ 32.738061] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
[ 32.760417] am65-cpsw-nuss 8000000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
[ 48.616255] audit: type=1334 audit(1651173098.304:6): prog-id=9 op=LOAD
[ 48.628430] audit: type=1334 audit(1651173098.312:7): prog-id=10 op=LOAD
[ 49.050768] audit: type=1006 audit(1651173098.736:8): pid=427 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=1 res=1
[ 49.084091] audit: type=1300 audit(1651173098.736:8): arch=c00000b7 syscall=64 success=yes exit=1 a0=8 a1=fffffeea6f88 a2=1 a3=0 items=0 ppid=1 pid=427 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0)
[ 49.125047] audit: type=1327 audit(1651173098.736:8): proctitle="(systemd)"
[ 49.140268] audit: type=1334 audit(1651173098.824:9): prog-id=11 op=LOAD
[ 49.152643] audit: type=1300 audit(1651173098.824:9): arch=c00000b7 syscall=280 success=yes exit=8 a0=5 a1=ffffd6146060 a2=78 a3=0 items=0 ppid=1 pid=427 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid)
[ 49.183556] audit: type=1327 audit(1651173098.824:9): proctitle="(systemd)"
[ 49.199736] audit: type=1334 audit(1651173098.824:10): prog-id=11 op=UNLOAD
[ 49.213268] audit: type=1334 audit(1651173098.824:11): prog-id=12 op=LOAD
root@am62xx-evm:~#
CTRL-A Z for help | 115200 8N1 | NOR | Minicom 2.7.1 | VT102 | Offline | ttyUSB0

Thanks,

Naresh

0 件の賞賛
返信

20,854件の閲覧回数
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @naresh_nakka 

Thanks for sharing me your full logs.

From your full dmesg log, I saw that Wi-Fi card is detected, and you are using mmc2 for Wi-Fi card.

Can you please let me know which driver and which FW are you using? You can share to me your download command.

It might be the Driver/FW you are using doesn't fit on your host Linux version 6.1.33.

Also, please check the VIO_SD, whether is fit with your host side.

I checked the Murata 1XK Wi-Fi+ Bluetooth Module Datasheet, it should be 1.8V when it is working in DDR50 Mode.

 

Best regards,

Christine.

0 件の賞賛
返信

20,847件の閲覧回数
naresh_nakka
Contributor I

Hi ,

downloaded IW416 driver from github: git clone https://github.com/nxp-imx/mwifiex.git 

switched to lf-6.1.36_2.1.0 and compiled the drivers.

please download Firmware from github: git clone https://github.com/NXP/imx-firmware.git 

my kernel verison is 6.1.33

steps followed to enable WIFI :

compile  wifi driver : 
move to 6.1.36. barnch  
add CROSS_COMPILE and KENELDIR  
change pwd as shell pwd 
and compile the wifi drivers 

Load : 

insmod cfg80211.ko  
insmod mac80211.ko  
insmod mlan.ko 
insmod moal.ko cal_data_cfg=none 

=> when i used to load eralier that time it was worked for me

root@am62xx-evm:/home# insmod cfg80211.ko  

[   51.308487] cfg80211: Loading compiled-in X.509 certificates for regulatory database 

[   51.336917] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7' 

[   51.344688] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2 

root@am62xx-evm:/home# [   51.359055] cfg80211: failed to load regulatory.db 

      

root@am62xx-evm:/home#  

root@am62xx-evm:/home# insmod mac80211.ko  

 

root@am62xx-evm:/home# insmod mlan.ko  

[   61.719068] mlan: loading out-of-tree module taints kernel. 

 

root@am62xx-evm:/home# ifconfig -a 

eth0      Link encap:Ethernet  HWaddr 34:08:E1:87:A8:9F   

          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1 

          RX packets:0 errors:0 dropped:0 overruns:0 frame:0 

          TX packets:6 errors:0 dropped:0 overruns:0 carrier:0 

          collisions:0 txqueuelen:1000  

          RX bytes:0 (0.0 B)  TX bytes:2004 (1.9 KiB) 

  

eth1      Link encap:Ethernet  HWaddr 96:27:08:A0:AB:BC   

          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1 

          RX packets:0 errors:0 dropped:0 overruns:0 frame:0 

          TX packets:6 errors:0 dropped:0 overruns:0 carrier:0 

          collisions:0 txqueuelen:1000  

          RX bytes:0 (0.0 B)  TX bytes:2004 (1.9 KiB) 

  

lo        Link encap:Local Loopback   

          inet addr:127.0.0.1  Mask:255.0.0.0 

          UP LOOPBACK RUNNING  MTU:65536  Metric:1 

          RX packets:90 errors:0 dropped:0 overruns:0 frame:0 

          TX packets:90 errors:0 dropped:0 overruns:0 carrier:0 

          collisions:0 txqueuelen:1000  

          RX bytes:6824 (6.6 KiB)  TX bytes:6824 (6.6 KiB) 

 

root@am62xx-evm:/home# insmod moal.ko cal_data_cfg=none                                                                                

[  144.689146] wlan: Loading MWLAN driver 

[  144.693492] wlan: Register to Bus Driver... 

[  144.780463] vendor=0x02DF device=0x9159 class=0 function=1 

[  144.786205] Attach moal handle ops, card interface type: 0x108 

[  144.792846] rps set to 0 from module param 

[  144.797349] No module param cfg file specified 

[  144.802377] SDIO: max_segs=128 max_seg_size=65536 

[  144.807483] rx_work=1 cpu_num=4 

[  144.811444] Attach mlan adapter operations.card_type is 0x108. 

[  144.818731] wlan: Enable TX SG mode 

[  144.822618] wlan: Enable RX SG mode 

[  144.829926] Request firmware: nxp/sduartiw416_combo.bin 

[  144.836726] WLAN FW already running! Skip FW download 

[  144.842582] WLAN FW is active 

[  144.845549] on_time is 144647979935 

[  144.870237] FW country code WW does not match with US 

[  144.875535] fw_cap_info=0x187c4f03, dev_cap_mask=0xffffffff 

[  144.881647] max_p2p_conn = 8, max_sta_conn = 8 

[  144.913720] Register NXP 802.11 Adapter mlan0 

[  144.927591] Register NXP 802.11 Adapter uap0 

[  144.943618] Register NXP 802.11 Adapter wfd0 

[  144.951794] wlan: version = SDIW416---16.92.21.p55.3-MM6X16408.p2-GPL-(FP92)  

[  144.966890] wlan: Register to Bus Driver Done 

[  144.976151] wlan: Driver loaded successfully 

root@am62xx-evm:/home#  

root@am62xx-evm:/home# ifconfig -a 

eth0      Link encap:Ethernet  HWaddr 34:08:E1:87:A8:9F   

          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1 

          RX packets:0 errors:0 dropped:0 overruns:0 frame:0 

          TX packets:7 errors:0 dropped:0 overruns:0 carrier:0 

          collisions:0 txqueuelen:1000  

          RX bytes:0 (0.0 B)  TX bytes:2338 (2.2 KiB) 

  

eth1      Link encap:Ethernet  HWaddr 96:27:08:A0:AB:BC   

          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1 

          RX packets:0 errors:0 dropped:0 overruns:0 frame:0 

          TX packets:10 errors:0 dropped:0 overruns:0 carrier:0 

          collisions:0 txqueuelen:1000  

          RX bytes:0 (0.0 B)  TX bytes:3340 (3.2 KiB) 

  

lo        Link encap:Local Loopback   

          inet addr:127.0.0.1  Mask:255.0.0.0 

          UP LOOPBACK RUNNING  MTU:65536  Metric:1 

          RX packets:90 errors:0 dropped:0 overruns:0 frame:0 

          TX packets:90 errors:0 dropped:0 overruns:0 carrier:0 

          collisions:0 txqueuelen:1000  

          RX bytes:6824 (6.6 KiB)  TX bytes:6824 (6.6 KiB) 

  

mlan0     Link encap:Ethernet  HWaddr 04:C4:61:AC:81:25   

          BROADCAST MULTICAST  MTU:1500  Metric:1 

          RX packets:0 errors:0 dropped:0 overruns:0 frame:0 

          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0 

          collisions:0 txqueuelen:1000  

          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B) 

  

uap0      Link encap:Ethernet  HWaddr 06:C4:61:AC:82:25   

          BROADCAST MULTICAST  MTU:1500  Metric:1 

          RX packets:0 errors:0 dropped:0 overruns:0 frame:0 

          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0 

          collisions:0 txqueuelen:1000  

          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B) 

  

wfd0      Link encap:Ethernet  HWaddr 06:C4:61:AC:81:25   

          BROADCAST MULTICAST  MTU:1500  Metric:1 

          RX packets:0 errors:0 dropped:0 overruns:0 frame:0 

          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0 

          collisions:0 txqueuelen:1000  

          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B) 

 

Thanks,

Naresh

 

0 件の賞賛
返信

20,838件の閲覧回数
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @naresh_nakka 

Thanks for sharing me your driver and FW info.

Yes, from this time logs, I see that Wi-Fi driver is loaded successfully.

It is so strange. May I know the issue frequency? 

I will also have a try on my local side with your given Driver and FW version. Hope I can reproduce on my side.

Best regards,

Christine.

0 件の賞賛
返信

20,819件の閲覧回数
naresh_nakka
Contributor I

Hi , 

now this issue getting everytime .

Thanks,

Naresh

0 件の賞賛
返信

20,806件の閲覧回数
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @naresh_nakka 

How about reboot your host MPU and re-load again?

 

Best regards,

Christine.

タグ(1)
0 件の賞賛
返信

20,802件の閲覧回数
naresh_nakka
Contributor I

Hi ,

Thank you so much for your quick response 

This is I am not sure .

Could you please tell me how to do .

In my shell reboot is not working 

Thanks ,

Naresh

0 件の賞賛
返信

20,797件の閲覧回数
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @naresh_nakka 

If reboot command doesn't work, can you please just power your board off and power it on again to have a try?

I am not familiar with your host side operations, but I think usually power off/on should work for Linux.

 

Best regards,

Christine

タグ(1)
0 件の賞賛
返信

20,792件の閲覧回数
naresh_nakka
Contributor I

Hi Christine , 

no , it's not working  after power cycle .

Thanks , Naresh .

0 件の賞賛
返信

20,787件の閲覧回数
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @naresh_nakka 

Thanks for your quick reply.

Do you remember what did you do between "Work fine" and "Doesn't work"?

How about copy again the FW from the download link to your /lib/firmware/nxp/  after reboot your board?

The given logs show that "Download FW failed". Maybe the FW is damaged by something we don't know.

 

Best regards,

Christine.

タグ(1)
0 件の賞賛
返信

20,751件の閲覧回数
naresh_nakka
Contributor I

Hi Christine , 

thanks for your response ,

actually i tried again downloading firmwre and loading to board 

again getting same issue .

Do you remember what did you do between "Work fine" and "Doesn't work"?   => i didnt do nothing .

 

 

Thanks,

Naresh.

0 件の賞賛
返信

20,681件の閲覧回数
naresh_nakka
Contributor I

HI Christine ,

small query on wifi .

sometimes its asking other firmware name . if we rename the current firmware name and load the mol.ko then its loading . why firmware name changing ?

#insmod moal.ko cal_data_cfg=none

[ 981.630133] wlan: Unloading MWLAN driver
[ 981.793928] Free module params
[ 981.797810] wlan: Driver unloaded
[ 981.895237] wlan: Loading MWLAN driver
[ 981.906297] wlan: Register to Bus Driver...
[ 981.997708] vendor=0x02DF device=0x9159 class=0 function=1
[ 982.009911] Attach moal handle ops, card interface type: 0x108
[ 982.021777] rps set to 0 from module param
[ 982.029324] No module param cfg file specified
[ 982.039864] SDIO: max_segs=128 max_seg_size=65536
[ 982.048338] rx_work=1 cpu_num=4
[ 982.055136] Attach mlan adapter operations.card_type is 0x108.
[ 982.068018] wlan: Enable TX SG mode
[ 982.077089] wlan: Enable RX SG mode
[ 982.094890] Request firmware: nxp/sdsdiw416_combo.bin
[ 982.106495] WLAN FW already running! Skip FW download
[ 982.120016] WLAN FW is active
[ 982.124213] on_time is 981914629425
[ 982.149374] FW country code WW does not match with US
[ 982.154679] fw_cap_info=0x187c4f03, dev_cap_mask=0xffffffff
[ 982.160825] max_p2p_conn = 8, max_sta_conn = 8
[ 982.186148] Register NXP 802.11 Adapter mlan0
[ 982.198743] Register NXP 802.11 Adapter uap0
[ 982.212959] Register NXP 802.11 Adapter wfd0
[ 982.220706] wlan: version = SDIW416---16.92.21.p55.3-MM6X16408.p2-GPL-(FP92)
[ 982.237440] wlan: Register to Bus Driver Done
[ 982.245661] wlan: Driver loaded successfully

0 件の賞賛
返信

20,651件の閲覧回数
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @naresh_nakka 

sdsdiw416_combo.bin means: Wi-Fi is using SDIO interface and Bluetooth is also SDIO interface.

sdiouartiw416_combo_v0.bin means: Wi-Fi is using SDIO interface and Bluetooth is using UART interface.

The reason that showed different fw name is you didn't indicate which firmware you want to load when you insmod moal.ko Wi-Fi driver.

Please indicate fw_name when you load Wi-Fi driver.

Method1:

insmod moal.ko fw_serial=1 fw_name=nxp/sdiouartiw416_combo_v0.bin cal_data_cfg=none ps_mode=1 auto_ds=1 host_mlme=1

Method2:

 insmod moal.ko mod_para=nxp/wifi_mod_para.conf

and modify /lib/firmware/nxp/wifi_mod_para.conf to indicate the firmware you want to load:


SDIW416 = {
cfg80211_wext=0xf
max_vir_bss=1
cal_data_cfg=none
ps_mode=1
auto_ds=1
host_mlme=1
fw_name=nxp/sdiouartiw416_combo_v0.bin
}

Best regards,

Christine.

0 件の賞賛
返信