iw416 example power

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iw416 example power

2,915件の閲覧回数
rtwheato
Contributor II

i'm using the i.MX RT 1060 SDK along with the iw416, and when I load the evkmimxrt1060_wifi_webconfig example, with:

#define WIFI_IW416_BOARD_AW_AM457_USD
 
set in app_config.h.  the project builds, loads on to my 1060 EVK, and I'm able to connect to it using my smart phone.
 
however, the signal strength of the AP is very weak.  Only 1-2 bars when extremely close, and unusable when more than 5 ft away.
 
is there a way to increase the power or range?
ラベル(3)
0 件の賞賛
返信
3 返答(返信)

2,890件の閲覧回数
rtwheato
Contributor II

yes.  this particular module has a built in trace antenna.

0 件の賞賛
返信

2,869件の閲覧回数
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

I´m sorry for the late reply.

Could you please take a look to AN12918 available in the following route of your SDK bundle?

C:/…/SDK_2_12_0_EVK-MIMXRT1060\docs\wireless\Wi-Fi

There might be some Tx power configuration missing and this document might help you.

I hope this helps.

Best regards, Daniel.

0 件の賞賛
返信

2,898件の閲覧回数
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

Just to confirm, did you connect the respective antenna for the Wi-Fi Tx/Rx in the AW-AM457-uSD module?

Best regards, Daniel.

0 件の賞賛
返信