Dear @Sanjiv_Mns ,
I built imx-image-multimedia based on L6.12.49.2.2.0 yocto source, run it on i.mx8mp-evk.



The IW623 module I am using is AW-XM729-PUR, which is M.2 module with PCIE interface.
If you are using SDIO interface for WIFI, the dtb file should be imx8mp-evk-usdhc1-m2.dtb
then run:
# modprobe btnxpuart
#hciconfig -a
hci0 interface will be listed.
[Note]
Default driver in imx-image-multimedia supports IW623, It uses AW693 firmware.
Thanks!
Regards,
Weidong