FRDM-RW612 - Getting USB device error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-RW612 - Getting USB device error

2,071 Views
pratikpanchal44
Contributor II

I am using FRDM-RW612 for my project. I have connected barcode scanner module on USB device to my FRDM board. Barcode scanner has USB HID support. 

Now, I am getting an error continuously as per below, once I scan any barcode.

=====================================

runwaitState 10,deviceState 1, usb status 0USB_HostKeyboardProcessBuffer means data recvd
===================================

Currently, I am using the SDK version SDK_25.06.00_FRDM-RW612.

Please advise. 

Tags (1)
0 Kudos
Reply
5 Replies

1,897 Views
pratikpanchal44
Contributor II

Hello Team,

Thanks for the solution. 

Currently, the system is working fine, and we found a problem on the device side. 

1,882 Views
RomanVR
NXP Employee
NXP Employee

Hello @pratikpanchal44.

Thanks for letting us know that the issue has been solved.

Best Regards!
0 Kudos
Reply

2,017 Views
pratikpanchal44
Contributor II

Hello @Ricardo_Zamora 

We have used the keyboard-mouse USB HID example in our device.

0 Kudos
Reply

1,968 Views
RomanVR
NXP Employee
NXP Employee

Hello @pratikpanchal44, hope you are doing well.

Could you please confirm which modifications (if any) were done to the project? Is your device being detected by the host (FRDM-RW612)?

Additionally, please notice that this example only supports three types of devices:

  • Single mouse or single keyboard devices.
  • Composite device containing one mouse and one keyboard.
  • HUBs connected with one mouse and one keyboard.

Any further development to add more supported devices will have to be done on the customer side, however if any further support is needed, feel free to reach us.

Best Regards!
0 Kudos
Reply

2,030 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello @pratikpanchal44 , hope you are doing well.

Could you please specify which USB HID example are you using and the modifications done to it?

Also please confirm if the example runs properly as is.

 

Best Regards,

Ricardo

0 Kudos
Reply