Does IW416 support WiFI AP + STA mode simultaneously ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does IW416 support WiFI AP + STA mode simultaneously ?

2,726 Views
Jai_L
Contributor I

Hi There,

Can someone help me to get the information regarding #IW416
We'll be having an requirement for WiFi AP + STA mode simultaneously.

Does #IW416 support the same
Help will be highly appreciated.

Best Regards,

Jay L.

Labels (2)
Tags (1)
0 Kudos
Reply
3 Replies

2,693 Views
nxf77486
NXP TechSupport
NXP TechSupport

Hello,

Thank you in advance for contacting NXP support.

The IW416 support AP + STA according to the document NXP Wi-Fi Driver Features and Release Notes (find the link below) please let me know if there is anything else where I can help you.

https://www.nxp.com/webapp/Download?colCode=L5.15.71_2.2.0_WIFI-Doc 

2,682 Views
Jai_L
Contributor I

Hello,

Thanks for the reply.

Actually, as per our requirements we need up to 50 stations that can be connected to AP mode. so, does IW416 support the same number of connections?

Thanks.

0 Kudos
Reply

2,670 Views
rtwheato
Contributor II

the # of clients the AP can support will mostly depend on your host system's performance.  but, IIRC, the iw416 should support up to 64 clients.

CEL has an iw416 based module available, contact me or @bruce_havemeier if you'd like more details.

0 Kudos
Reply