Create Key & Certificate for HTTPS Server using IP on Windows

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Create Key & Certificate for HTTPS Server using IP on Windows

Create Key & Certificate for HTTPS Server using IP on Windows

Introduction


HTTP is a protocol used to enable communication between web browsers and servers. A secure variation of this protocol is HTTPS, which adds encryption to protect data exchanged between the client and the server. This ensures that even if someone intercepts the communication, they cannot understand the transmitted information.

In embedded systems and MCU-based applications, libraries such as mbedTLS are commonly used to implement secure communication. These libraries rely on cryptographic keys and digital certificates.

For production environments, certificates are typically signed by a Certificate Authority (CA), which guarantees their authenticity and allows web browsers to trust the connection. However, when a certificate is generated manually (self-signed), web browsers do not inherently trust it. Despite this, self-signed certificates are a practical option for internal or development use cases, since the communication remains encrypted. Additionally, it is possible to configure client devices to trust these certificates when required.

 

Download OpenSSL


First, verify whether OpenSSL is installed on your system. If not, it must be downloaded and installed.
To check if OpenSSL is already installed, run next line in command prompt:

openssl --version
If the command is not recognized, OpenSSL is not installed.
If OpenSSL is not already installed on your system, you can easily find installation instructions by searching the web for your specific operating system. There are many reliable step‑by‑step guides available for Windows, Linux, and macOS that explain how to download, install, and verify OpenSSL properly. Following an up‑to‑date guide for your OS will help ensure the installation is completed correctly and securely.
 

Preparation


Select a folder where all keys and certificates will be stored. Open a command prompt in this folder and proceed with the following steps.
 

Create Keys


NOTE: Please replace %%Name%% according to your preference.
Create a private key for the Server Certificate

openssl genrsa -out %%KeyName%%.key 2048

Create a private key to simulate Certificate Authority (CA)

openssl genrsa -out %%CAKeyName%%.key 2048

 

Create Certificate Authority


Generate a self-signed CA certificate:

openssl req -x509 -new -nodes -key %%CAKeyName%%.key -sha256 -days 3650 -out %%CAName%%.crt

 

Create Server Certificate


Config file to request certificate

Create a configuration file named %%ConfigFileName%%.cnf using the following template, this can be created with Notepad.
[req]
default_bits = 2048
prompt = no
distinguished_name = dn
req_extensions = v3_req

[dn]
C=%%Country%%
ST=%%State%%
L=%%City%%
O=%%Owner%%
OU=%%Division%%
CN=%%CommonName%%

[v3_req]
subjectAltName = @alt_names

[alt_names]
IP.1 = %%ServerIP%%

Generate Certificate Signing Request (CSR)

openssl req -new -key %%KeyName%%.key -out %%CertificateRequestName%%.csr -config %%ConfigFileName%%.cnf

Sign Certificate with simulated CA

openssl x509 -req -in %%CertificateRequestName%%.csr -CA %%CAName%%.crt -CAkey %%CAKeyName%%.key -CAcreateserial -out %%CertificateName%%.crt -days 365 -extensions v3_req -extfile %%ConfigFileName%%.cnf

 

Prepare to use with mbedTLS


Convert private Key to DER (Distinguished Encoding Rules)

openssl rsa  -in %%KeyName%%.key -outform DER -out %%KeyName%%_key.der

Convert Certificate to DER (Distinguished Encoding Rules)

openssl x509 -in %%CertificateName%%.crt -outform DER -out %%CertificateName%%.der

Convert Key DER to array in a source file

xxd -i %%KeyName%%_key.der > %%KeyName%%_key.c

Convert Certificate DER to array in a source file

xxd -i %%CertificateName%%.der > %%CertificateName%%_cert.c

 

Install CA Certificate (Optional – Avoid Browser Warnings)


To prevent browser warnings, install the CA certificate on the client device (PC, phone, etc.).

  1. Double-click the CA certificate file (.crt).
  2. Click Install Certificate.
  3. Select Local Machine.
  4. Choose Place all certificates in the following store.
  5. Click Browse and select Trusted Root Certification Authorities.
  6. Click Next → Finish.

After this step, the system will trust certificates signed by this CA.

評価なし
バージョン履歴
最終更新日:
‎06-29-2026 09:17 AM
更新者: