I'm currently working with the NXP MAYA-W271-00B (IW612) , and I wanted to confirm whether it supports the Zigbee protocol in addition to Wi-Fi and Bluetooth. If Zigbee is supported, could anyone point me to the appropriate resources or provide guidance on where I might find the Linux driver or any necessary integration details?
Any help or direction would be greatly appreciated!
Thanks in advance!
已解决! 转到解答。
Hi, @Abhilasha
Thanks for creating case to us.
For IW612, yes, except Bluetooth and Wi-Fi, it also supported Zigbee which is based on 802.15.4.
To use IW612's Zigbee based on Linux, you can refer to below guide:
Getting Started with NXP-based Wireless Modules on i.MX 8M Quad EVK Running Linux OS - User manual
To get the latest IW612's driver, you can download it through below link:
https://github.com/nxp-imx/mwifiex/tree/lf-6.6.36_2.1.0
To get the latest IW612's FW, you can download it through below link:
https://github.com/nxp-imx/imx-firmware/tree/lf-6.6.36_2.1.0/nxp/FwImage_IW612_SD
Please do not hesitate to mark my answer as a solution, if it really does help for you.
For other topic's queries or questions, please feel free to create new case to us.
Have a nice day~
Best regards,
Christine.
Hi, @Abhilasha
Thanks for creating case to us.
For IW612, yes, except Bluetooth and Wi-Fi, it also supported Zigbee which is based on 802.15.4.
To use IW612's Zigbee based on Linux, you can refer to below guide:
Getting Started with NXP-based Wireless Modules on i.MX 8M Quad EVK Running Linux OS - User manual
To get the latest IW612's driver, you can download it through below link:
https://github.com/nxp-imx/mwifiex/tree/lf-6.6.36_2.1.0
To get the latest IW612's FW, you can download it through below link:
https://github.com/nxp-imx/imx-firmware/tree/lf-6.6.36_2.1.0/nxp/FwImage_IW612_SD
Please do not hesitate to mark my answer as a solution, if it really does help for you.
For other topic's queries or questions, please feel free to create new case to us.
Have a nice day~
Best regards,
Christine.
Hi, @Abhilasha
It needs secure files access to get download permission.
You can download the driver and FW through my given links, which doesn't need secure files access.
Best regards,
Christine.
Hi, @Abhilasha
The driver link I shared to you yesterday should include drivers which supports Zigbee.
But I checked the information in our user manual, it mentioned that:
8 Bring-up of ZigBee on i.MX 8M Mini
This section shows how to bring up ZigBee on i.MX 8M Mini EVK platform.
Note: The 802.15.4 subsystem is only supported on IW612 evaluation board (EVB) with i.MX 8M Mini(8MMINILPD4-EVK@2020) host platform. This section describes the steps to bring up the 802.15.4 interface of NXP-based IW612 module on i.MX 8M Mini platform, and for Zigbee-only mode. Zigbee dual-pan mode is not supported.
So, please make sure whether you are using our I.Mx8M Mini (8MMINILPD4-EVK@2020) host platform.
If not, I worry, it might not support.
Sorry for the inconvenience to you.
Best regards,
Christine.
Hi, @Abhilasha
As my previous comments,
To get the latest IW612's Wi-Fi driver, you can download it through below link:
https://github.com/nxp-imx/mwifiex/tree/lf-6.6.36_2.1.0
To get the latest IW612's FW, you can download it through below link:
https://github.com/nxp-imx/imx-firmware/tree/lf-6.6.36_2.1.0/nxp/FwImage_IW612_SD
The 802.15.4 subsystem is only supported on IW612 evaluation board (EVB) with i.MX 8M Mini(8MMINILPD4-EVK@2020) host platform.
Are you using our I.MX8MMini as your host platform?
If yes, please refer to below guide: Section 7 7 Bring-up of 802.15.4 and Section 8 Bring-up of ZigBee on i.MX 8M Mini.
Getting Started with NXP-based Wireless Modules on i.MX 8M Quad EVK Running Linux OS - User manual
If no, I worry Zigbee is not supported on your other host platform currently.
We also have below user manual as a guidance for customers to download and build our Wi-Fi drivers:
How to Download and Build NXP Wi-Fi Drivers - User manual (restricted)
About device tree, I think you can refer to our I.MX8MMini's device tree to configure yours according to your SDIO interface hardware connections:
Hope it can help you somehow.
Have a nice day~
Best regards,
Christine.