What is the state of PTA9 after a reset

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the state of PTA9 after a reset

1,153件の閲覧回数
richardcopeman
Contributor II

After a reset what is the default function of pin PTA9 on the TWR-VF65GS10 board?

ラベル(1)
0 件の賞賛
返信
1 返信

1,046件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  According to table in section 12.1 (Pinouts) of the Vybrid Datasheet,

default function of PTA9 is JTDI. 

https://www.nxp.com/docs/en/data-sheet/VYBRIDFSERIESEC.pdf 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信