Vybrid NAND Flash Controller (NFC) documentation ambiguity

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Vybrid NAND Flash Controller (NFC) documentation ambiguity

11,406 Views
alanball
Contributor III

Referring to  VYBRIDRM Rev 7, 06/2014:

Page 860: NAND Boot eFuse config appears to allow only 2 or 3 address cycles. Larger NAND devices require 4 or 5 cycles - does this mean I can't boot from them ?

13 Replies

10,622 Views
sinanakman
Senior Contributor III

Hi Alan

Stefan Agner has some good experience

on Vybrid NAND. You might want to ping

him as well.

Regards

Sinan Akman

0 Kudos
Reply

10,622 Views
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport do you have an update of this case?

0 Kudos
Reply

10,622 Views
billpringlemeir
Contributor V

Hi Karina.

I think the issue is solved, but the original poster (Alan) doesn't know who solved it (and neither do I).  Also, it seems that the Freescale Vybrid document dropped an XLS spreadsheet and Page 860: NAND Boot eFuse should probably be more specific about 'address cycle'.  Memory people often think of devices as an array with Columns and rows, but most of the rest of us think of it as a linear device.  So if you want to follow up, a ticket/SR to the documentation people is probably better.

Page 860: NAND Boot eFuse  - 2 ROW address cycles (four address cycles total)

                                              - 3 ROW address cycles (five address cycles total)

I would also appreciate a 'ping' in this thread,

VF6xxx NFC (NAND) module clocking

I still don't think we have an answer?

0 Kudos
Reply

10,622 Views
karina_valencia
NXP Apps Support
NXP Apps Support

Thank  Bill for your update on this  case. Based to the other  case you mentioned, can you create a new case with  this link as a reference and   add the current status please?

0 Kudos
Reply

10,622 Views
billpringlemeir
Contributor V

Did you have a data sheet on the 4/5 cycle chips?  Is it possible that they support a 3 cycle that only reads the first ~16MB.  You need to use a 3 cycle read command (also read command fues) and the boot code must be in the first ~16MB.  After you boot, you could try to access > 16MB with a 4/5 cycle command.  At least that is just some guessing and not an official answer, but seems to make some technical sense.

0 Kudos
Reply

10,622 Views
alanball
Contributor III

Hi Bill

Datasheet (these are Spansion parts as it happens) says :

The Address Input bus operation allows the insertion of the memory address. For the S34ML02G1 and

S34ML04G1 devices, five write cycles are needed to input the addresses. For the S34ML01G1, four write

cycles are needed to input the addresses

Fair enough, the last one or two cycles are for high order row address, but there's nothing that states you can do a short load and the upper bits will then default to zero.

I note the Vybrid Tower uses a NAND chip (Micron) that implies the same thing , and I *assume* that must work...

0 Kudos
Reply

10,622 Views
billpringlemeir
Contributor V

Sorry I did not reflect on your question enough, I am not certain what the Page 860: NAND Boot eFuse refers to.  I think that the NFC controller always runs a five address cycle for normal reads.  See for instance, pg 1297 and NFC_CMD2:CODE.  Nand Flash boot on the Vybrid tower does work without changing any fuses.  I am pretty sure that the JEDEC NAND standard will specify a read like this (5 cycles).  The low level details are completely controlled by the NFC and there is no documented programmer control of this besides the 'NFC_CMD2:CODE'.  Ie, most of the raw cycles are outside the ARM/software control.  Other Nand controller issue each cycle individually.  All of the different Linux/U-boot/MQX 'NFC' drivers use the same 'NFC_CMD2:CODE' value (so five cycle read).

The question would be what does 'cycle' refer to in the Boot/eFuse document.

0 Kudos
Reply

10,622 Views
falstaff
Senior Contributor I

Hi,

In RM rev. 5, there was a document attached with the name "Fuse-RCON Mapping.xlsx". In this document, you find the following descrption regarding this fuse (BOOT_CFG1[1:0]):

Nand_Row_address_bytes:

00 - 3

01 - 2

10 - Reserved

11 - Reserved

I think this is not the cycle count of reads... Bill, you probably have a better understanding what this exactly means...

10,622 Views
billpringlemeir
Contributor V

Yes, I am not really sure Fuse-RCON Mapping.xlsx is much more helpful; the info is a lot the same as Page 860: NAND Boot eFuse.  There are these threads,

Understanding VYBRID NAND Boot

Re: Vybrid NAND boot

Arrgh.  I guess the 'Fuse-RCON' may have the secret sauce if you read really carefully,

   0x00 col1 col2  row1 row2 row3 0x30  -> Five cycle (or 3 ROWS)

   0x00 col1 col2  row1 row2 0x30  -> Four cycle (or 2 ROWS)

So I think that the Spansion 1G is 2 cycle, but the others are three.  That is just a guess.  Fuse defaults are zero and the Micron chip on the tower board with NAND boot with things setup as "3 Row cycles".  Pg860 should definitely mention ROWS.

10,623 Views
alanball
Contributor III

Bill

Thanks - it starts to make sense

Do you know where I can get hold of Fuse-RCON_Mapping - it appears to not be attached to v7 of the manual ?

Alan

0 Kudos
Reply

10,613 Views
falstaff
Senior Contributor I

Thanks Bill for the clarification. Fwiw, we use 00 for Macronix 1Gb/4Gb NAND chips.

File is attached.

10,613 Views
alanball
Contributor III

Thanks Stefan (and Bill) - good to know there's lively, helpful support backing these parts :smileyhappy:

Alan

0 Kudos
Reply

10,613 Views
naoumgitnik
Senior Contributor V

Dear Alan,

I am not a SW person but the first question coming to my mind is "How does Freescale's code operate in this case"? If help needed with that, I hope timesyssupport (i.e. the code author) will be able to help you with that.

Sincerely, Naoum Gitnik.

0 Kudos
Reply