Vybrid HAB Setup

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Vybrid HAB Setup

5,305 次查看
rmcginnis
Contributor I

Hello,

We are utilizing the Vybrid VF6xxx processor and have requirements to support HAB for our application.  Are there any app-notes or how-to's related to HAB specifically related to the Vybrid?  (I've located how-to's for HAB related to the iMX6 e.g.  -How-to enable HAB in i.MX6x... but nothing specific to Vybrid) 

Thanks,

Ryan

标签 (2)
标记 (2)
10 回复数

4,043 次查看
rogeriomachado
Contributor I

See: https://www.freescale.com/files/training_pdf/FTF/2012/americas/WBNR__FTF12_ENT_F0043.pdf

and http://www.freescale.com/webapp/sps/site/training_information.jsp?code=WBNR_FTF12_ENT_F0043#

High assurance boot - Tools

Code Signing Tool:

− Offline process of creating digital Signature

− Signing Keys and signatures generated by device manufacturers

− Supports code signing for: Vybrid

• Manufacturing Tool:

− Platform software provisioning

− One-Time Programmable e-fuse programming

• Both can be downloaded from (coming soon):

www.freescale.com/vybrid

0 项奖励
回复

4,043 次查看
jackblather
Senior Contributor I

I have a number of questions.

Any updates on this?

Is the Code Signing Tool (CST) complete or nearing completion?

Is there a time estimate when I can have tools and documents in my hands to boot securely and protect my and my customers' IP?

On slide 64 of the link in the prior post, it mentions: "Support for Vybrid encrypted boot." and "Support for MQX apart for Linux". Does anybody have an idea when this might be available?

Will the Vybrid HAB/CAAM/etc be similar to that in the iMX6?

Thanks.

0 项奖励
回复

4,043 次查看
ryanm_
Contributor II

Jack,

I was able to get HAB to work with the Vybrid.  The current CST software worked for signing the binary program image without any issues.  As far as documentation goes I used the IMX6 documentation to get things working with the Vybrid.  With respect to HAB both parts seem to be pretty similar.

-Ryan

4,043 次查看
jackblather
Senior Contributor I

Ryan,

Sweet, I'll start downloading the iMX6 CST software and documentation.

Thanks!

0 项奖励
回复

4,043 次查看
timesyssupport
Senior Contributor II

Hello,

We are still without suitable hardware for testing. We have ordered additional Tower Modules of the current revision, but the hardware we do have on hand is still travelling for training purposes.

I am hopeful that we can obtain hardware for validation next week, 9-29.

Regards,

Timesys Support

0 项奖励
回复

4,043 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

Thanks  for let us know.

0 项奖励
回复

4,043 次查看
timesyssupport
Senior Contributor II

Hello Ryan,

We have not yet validated/tested HAB on the Vybrid; we are reviewing currently for support in the Vybrid kernel and U-boot. Once we have determined if the support is available, we will follow up with a roadmap.

Regards,

Timesys Support

4,043 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you provide an estimated due date?

0 项奖励
回复

4,043 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

Timesys Support can you provide an estimated due date?

0 项奖励
回复

4,043 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport are you available to help on this case?

0 项奖励
回复