UBI not mountable after changing ECC and NFC Driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UBI not mountable after changing ECC and NFC Driver

6,481件の閲覧回数
andreaszeiler
Contributor III

Hello,

we're trying to change the nfc driver for the vybrid processor. Drivers for NFC in Uboot are already changed. This works already and I'm able to write my own ECC where I want it to be.

In linux kernel I try the same thing. I changed the driver to support our ECC and raw reads. The problem now is that I'm getting an error message when I try to boot.

We're using ubi as filesystem. I writing the filesystem into TargetFS by Uboot. Also I make a ubi partition etc. Then I write the ubifs image into my ubi partition.

Uncompressing Linux... done, booting the kernel.

Linux version 3.0.15-F+S+ (zeiler@VBFedora14) (gcc version 4.7.2 (crosstool-NG 1.18.0 - for F+S boards and modules) ) #189 Wed May 28 14:50:32 CEST 2014

CPU: ARMv7 Processor [410fc051] revision 1 (ARMv7), cr=10c53c7d

CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine: F+S Elektronik Systeme GmbH, armStoneA5

Memory policy: ECC disabled, Data cache writeback

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 65024

Kernel command line: console=ttymxc1,115200 login_tty=ttymxc1,115200 mtdparts=NAND:256k(NBoot)ro,768k(UserDef),256k(Refresh)ro,512k(UBoot)ro,256k(UBootEnv)ro,4m(Kernel)ro,-(TargetFS) rootfstype=ubifs ubi.mtd=TargetFS root=ubi0:rootfs ro init=linuxrc

PID hash table entries: 1024 (order: 0, 4096 bytes)

Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)

Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)

Memory: 256MB = 256MB total

Memory: 254120k/254120k available, 8024k reserved, 0K highmem

Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

    DMA     : 0xf4600000 - 0xffe00000   ( 184 MB)

    vmalloc : 0x90800000 - 0xf2000000   (1560 MB)

    lowmem  : 0x80000000 - 0x90000000   ( 256 MB)

    modules : 0x7f000000 - 0x80000000   (  16 MB)

      .init : 0x80008000 - 0x8002e000   ( 152 kB)

      .text : 0x8002e000 - 0x80528000   (5096 kB)

      .data : 0x80528000 - 0x8055c860   ( 211 kB)

       .bss : 0x8055c884 - 0x80599a08   ( 245 kB)

SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1

NR_IRQS:432

MVF GPIO hardware

sched_clock: 64 bits at 132MHz, resolution 7ns, wraps every 34359ms

Console: colour dummy device 80x30

Calibrating delay loop... 262.96 BogoMIPS (lpj=1314816)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

CPU: Testing write buffer coherency: ok

devtmpfs: initialized

NET: Registered protocol family 16

mcf_edma: Initialized successfully

armStoneA5 Board Rev. 1.10

Using UART1 for UART port A (TXD/RXD/RTS/CTS)

Using UART2 for UART port B (TXD/RXD)

Using UART3 for UART port C (TXD/RXD)

Booting on CPU #0 CA5 r0p1 on port #2, 2 CPU(s)

Level 1 cache: I: 32768 Bytes/2 ways, D: 32768 Bytes/4 ways

Level 2 cache: 0 bytes/0 ways

IMX usb wakeup probe. id=1

IMX usb wakeup probe. id=0

bio: create slab <bio-0> at 0

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

i2c-gpio i2c-gpio.4: using pins 119 (SDA) and 118 (SCL)

Advanced Linux Sound Architecture Driver Version 1.0.24.

Switching to clocksource global_timer

NET: Registered protocol family 2

IP route cache hash table entries: 2048 (order: 1, 8192 bytes)

TCP established hash table entries: 8192 (order: 4, 65536 bytes)

TCP bind hash table entries: 8192 (order: 3, 32768 bytes)

TCP: Hash tables configured (established 8192 bind 8192)

TCP reno registered

UDP hash table entries: 256 (order: 0, 4096 bytes)

UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

Static Power Management for Freescale Vybrid

PM driver module loaded

squashfs: version 4.0 (2009/01/31) Phillip Lougher

JFFS2 version 2.2. (NAND) (SUMMARY)  © 2001-2006 Red Hat, Inc.

ROMFS MTD (C) 2007 Red Hat, Inc.

msgmni has been set to 496

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

Console: switching to colour frame buffer device 100x60

fb0: Layer0 fb device registered successfully.

fb1:  fb device registered successfully.

fb2:  fb device registered successfully.

fb3:  fb device registered successfully.

Serial: MVF driver

IMX UART RTS/CTS enabled

IMX UART FIFO enabled

imx-uart.1: ttymxc1 at MMIO 0x40028000 (irq = 94) is a IMX

console [ttymxc1] enabled

IMX UART FIFO enabled

imx-uart.2: ttymxc2 at MMIO 0x40029000 (irq = 95) is a IMX

IMX UART FIFO enabled

imx-uart.3: ttymxc3 at MMIO 0x4002a000 (irq = 96) is a IMX

brd: module loaded

loop: module loaded

at24 4-0050: 2048 byte 24c16 EEPROM, writable, 1 bytes/write

mvf-adc mvf-adc.0: attached adc driver

mvf-adc mvf-adc.1: attached adc driver

FSL NFC MTD nand Driver 1.0

NAND device: Manufacturer ID: 0x2c, Chip ID: 0xf1 (Micron NAND 128MiB 3,3V 8-bit)

Scanning device for bad blocks

Bad eraseblock 0 at 0x000000000000

Bad eraseblock 14 at 0x0000001c0000

7 cmdlinepart partitions found on MTD device NAND

Creating 7 MTD partitions on "NAND":

0x000000000000-0x000000040000 : "NBoot"

0x000000040000-0x000000100000 : "UserDef"

0x000000100000-0x000000140000 : "Refresh"

0x000000140000-0x0000001c0000 : "UBoot"

0x0000001c0000-0x000000200000 : "UBootEnv"

0x000000200000-0x000000600000 : "Kernel"

0x000000600000-0x000008000000 : "TargetFS"

UBI: attaching mtd6 to ubi0

UBI: physical eraseblock size:   131072 bytes (128 KiB)

UBI: logical eraseblock size:    126976 bytes

UBI: smallest flash I/O unit:    2048

UBI: VID header offset:          2048 (aligned 2048)

UBI: data offset:                4096

UBI: max. sequence number:       258

UBI: attached mtd6 to ubi0

UBI: MTD device name:            "TargetFS"

UBI: MTD device size:            122 MiB

UBI: number of good PEBs:        976

UBI: number of bad PEBs:         0

UBI: number of corrupted PEBs:   0

UBI: max. allowed volumes:       128

UBI: wear-leveling threshold:    4096

UBI: number of internal volumes: 1

UBI: number of user volumes:     1

UBI: available PEBs:             0

UBI: total number of reserved PEBs: 976

UBI: number of PEBs reserved for bad PEB handling: 9

UBI: max/mean erase counter: 4/1

UBI: image sequence number:  0

UBI: background thread "ubi_bgt0d" started, PID 530

Faraday DSPI DMA addr: Tx-0xffdff000[0x8a1ff000], Rx-0xffdfe000[0x8a1fe000]

DSPI: Coldfire master initialized

CAN device driver interface

flexcan netdevice driver

flexcan mvf-flexcan.0: device registered (reg_base=90920000, irq=90)

flexcan mvf-flexcan.1: device registered (reg_base=90928000, irq=91)

FEC Ethernet Driver

fec_enet_mii_bus: probed

fec_enet_mii_bus: probed

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller

fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1

fsl-ehci fsl-ehci.0: irq 108, io base 0x400b4000

fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00

usb usb1: New USB device found, idVendor=1d6b, idProduct=0002

usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1

usb usb1: Product: Freescale On-Chip EHCI Host Controller

usb usb1: Manufacturer: Linux 3.0.15-F+S+ ehci_hcd

usb usb1: SerialNumber: fsl-ehci.0

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

Initializing USB Mass Storage driver...

usbcore: registered new interface driver usb-storage

USB Mass Storage support registered.

ARC USBOTG Device Controller driver (1 August 2005)

gs_bind: controller 'fsl-usb2-udc' not recognized

g_serial gadget: Gadget Serial v2.4

g_serial gadget: g_serial ready

fsl-usb2-udc: bind to driver g_serial

mousedev: PS/2 mouse device common for all mice

sx8655 3-0048: sx8655_probe()

sx8655 3-0048: write mask fail

sx8655: probe of 3-0048 failed with error -5

sx8655 3-0049: sx8655_probe()

sx8655 3-0049: write mask fail

sx8655: probe of 3-0049 failed with error -5

snvs_rtc snvs_rtc.0: rtc core: registered snvs_rtc as rtc0

i2c /dev entries driver

Linux video capture interface: v2.00

usbcore: registered new interface driver uvcvideo

USB Video Class driver (v1.1.0)

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

sdhci sdhci-esdhc-imx.1: no write-protect pin available!

mmc0: SDHCI controller on platform [sdhci-esdhc-imx.1] using ADMA

pca9632_probe: done.

i2c-core: driver [pca9632] using legacy suspend method

i2c-core: driver [pca9632] using legacy resume method

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

sgtl5000 4-000a: sgtl5000 revision 17

asoc: sgtl5000 <-> mvf-sai.0 mapping ok

ALSA device list:

  #0: sgtl5000-sai

TCP cubic registered

NET: Registered protocol family 10

IPv6 over IPv4 tunneling driver

NET: Registered protocol family 17

can: controller area network core (rev 20090105 abi 8)

NET: Registered protocol family 29

can: raw protocol (rev 20090105)

can: broadcast manager protocol (rev 20090105 t)

Registering the dns_resolver key type

VFP support v0.3: implementor 41 architecture 2 part 30 variant 5 rev 1

g_serial gadget: high speed config #2: CDC ACM config

snvs_rtc snvs_rtc.0: setting system clock to 1970-01-01 05:52:58 UTC (21178)

UBIFS error (pid 1): ubifs_recover_master_node: failed to recover master node

List of all partitions:

1f00             256 mtdblock0  (driver?)

1f01             768 mtdblock1  (driver?)

1f02             256 mtdblock2  (driver?)

1f03             512 mtdblock3  (driver?)

1f04             256 mtdblock4  (driver?)

1f05            4096 mtdblock5  (driver?)

1f06          124928 mtdblock6  (driver?)

No filesystem could mount root, tried:  ubifs

Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)

Backtrace:

[<80036b00>] (dump_backtrace+0x0/0x108) from [<804096d8>] (dump_stack+0x18/0x1c)

r6:800254e8 r5:8ffed006 r4:8055cee0 r3:60000013

[<804096c0>] (dump_stack+0x0/0x1c) from [<80409a50>] (panic+0x5c/0x17c)

[<804099f4>] (panic+0x0/0x17c) from [<80008dd8>] (mount_block_root+0x1d4/0x218)

r3:8ffcff3c r2:804b9c5d r1:8ffcff68 r0:804af8ed

r7:8ba00e0d

[<80008c04>] (mount_block_root+0x0/0x218) from [<80009080>] (prepare_namespace+0x94/0x1c0)

[<80008fec>] (prepare_namespace+0x0/0x1c0) from [<800089ec>] (kernel_init+0xf0/0x11c)

r5:80024cd0 r4:80024cd0

[<800088fc>] (kernel_init+0x0/0x11c) from [<8004ae74>] (do_exit+0x0/0x5f8)

r5:800088fc r4:00000000

Seems that first ubi reads the whole Filesystempartition and then reads one block completely. So I get these error messages and a stack_dump.

Reading the pages from nand also seems to be ok and when I look at my ecc status flag everything is ok. we also check on empty pages. but we notice them and don't throw errors on that.

Does anyone know how to solve this? I have no idea!!!!

Kind regards

Andi

ラベル(9)
5 返答(返信)

3,429件の閲覧回数
andreaszeiler
Contributor III

Hi again,

I could build a rootfs.ubi image in buildroot. I write it with "nand write $loadaddr TargetFS $filesize" into nand. Now the kernel starts and boots. Also the kernel is able to mount rootfs. When I reboot the system it is working again.

But when I just mount my filesystem with rw I get read errors in next boot.

Seems that ubi write here something into fs...

andi

0 件の賞賛
返信

3,429件の閲覧回数
billpringlemeir
Contributor V

I suggest you at least look at the driver I referenced above.  You use hardware ECC, and the stock TimeSys driver has some errors; like it never actually tested that the ECC failed and hence when flash wears, it will report it good when it is really bad.  With the hardware ECC, you don't have a choice where it is placed.  The controller will write it automatically at the end of the OOB data.  It sounds like you have the reading working, but when you write, the hardware ECC may place data at the wrong point.  It is helpful to use nanddump with the oob information to get what the controller hw ecc wrote (and where).  The hardware ECC may attempt to correct data and fail.  It reports the status, which the stock Timesys driver doesn't handle because of the endian issue (see link above).  So, if the hardware ECC is not working, the first write/read may give some corrupt data, even though the MTD driver reports nothing.  Also, I am not sure about sub-page handling with the TimeSys (originally by Freescale) driver, which UBI/UbiFS wants to use.  This will also come into play on the first writes.

3,429件の閲覧回数
andreaszeiler
Contributor III

Hi,

thanks for reply.

We use custom boards. The thing is that we wanted to use hardware ecc with our own layout. The former UBoot driver of nfc could only write with ecc. Besides this I changed the layout but nothing has changed. I saw some changes in the oob area when I set ecc to 24bit ecc. But I couldn't see anything usefull in the oob. After I made some changes in the driver I could write raw and also I could set ecc to right place. We want ecc to start on byte 2052. We use 2k pages. So 2048 byte data + 4 byte BadBlockMarker etc. + 30Byte ecc and behind that some other stuff. We use 16bit ecc with 30byte length.

So these changes looked good to me.

I made also some changes in the linux kernel to be able to read the right ecc position, etc.

I use the "nand write $loadaddr Kernel $filesize" command to write linux kernel in uboot into Kernel partition. Then I run "ubi part TargetFS" to select TargetFS as Filesystem partition. After that I create a ubi intern partition called "rootfs" with command "ubi create rootfs". Into this "rootfs" I write the rootfs.ubifs Image which was build by buildroot. I use the command "ubi write $loadaddr rootfs $filesize".

Now, when I boot the linux kernel gets loaded and starts booting. Then I get the output which I posted above. I also print some pages and oob areas at bootup and also printed the ecc status byte. and this byte shows no errors. So I assume that the ubi partition should be read correctly?!?!

Do I have to configure something in my buildroot?? Is it possible that ubi writes into oob area? maybe I have some trouble there and it overwrites something?

Kind regards

andi

0 件の賞賛
返信

3,429件の閲覧回数
billpringlemeir
Contributor V

It definitely looks as if the Linux MTD's ECC doesn't agree with the U-Boot ECC.  For instance, I have the same message if I write a UBI partition with Software-ECC and then mount with Hardware-ECC.  Here is some conversation with Stefan Agner and I,

Stefan provides a link to 'U-boot' there that has an updated driver and there are other links to a Linux mainline driver.  It is fairly easy to back-port to the TimeSys kernel.   I think there are definite bugs/issues with the TimeSys version you seem to be using.  These community links might also be useful,

VF6xxx NFC (NAND) module clocking, VF5xx/ECCAD for NFC, and Vybrid NAND boot

I would compile the mtdtests as modules and load them to see if you have any issues.  Are you using the tower board or custom hardware?  Also, this statement seems wrong,

Then I write the ubifs image into my ubi partition.

Maybe I take it too literally.  You need to run 'ubinize' to convert a 'ubifs' image to a 'ubi' image.  So, from an initial directory, run 'mkfs.ubifs' and then on that image, run 'ubinize'.  This image can be written to flash using 'nandwrite' or other similar raw flashers.  I think UBI support is in some versions of u-boot, but if you wrote the wrong data, then the UBI headers will not be found and a similar error message will be printed.

UBI: max/mean erase counter: 4/1

I guess this means it is not your issue, it seems that something found some UBI headers to get an erase count of '4'.

Boot from an MMC card, if on the tower board, or create an initramfs (buildroot/klibc) and then you can probe the ubifs root partition from the ram disk.

0 件の賞賛
返信

3,429件の閲覧回数
Nouchi
Senior Contributor II

Hello,

Did you try to install your ubi volume from linux (not from u-boot) ?

Then mount ubi to see if it works.

You can also use nand write.trimffs with u-boot to install ubi volume. U-boot must be compiled with CONFIG_CMD_NAND_TRIMFFS option.

Emmanuel