UART register description missing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UART register description missing

2,210 Views
falstaff
Senior Contributor I

In the Vybrid Reference Manual Rev. 7 (06/2014) the following registers have been part of chapter 49 (UART):

  • UARTx_C5
  • UARTx_MODEM
  • UARTx_WP7816T0

In Rev. 8 (11/2015) and newer Vybrid Reference Manual those registers are missing.

In Rev. 8 (11/2015) Appendix A: Revision History for VFxxx Controller F-Series Reference Manual most changes are documented. However, there is no UART change mentioned... I assume this was an oversight? Or have they been removed intentionally (issues/not recommended to use or similar)?

Labels (2)
Tags (2)
1 Reply

1,867 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Stefan,

We've searched the change history of the RM and don't see any official change to remove them.

 

The documentation team is already aware of this and we will see if the erroneous changes can be backed out in the next rev of the manual.

Thank you!


Regards,
Carlos
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------